Skip to main content
Associate
Aug 29, 2025 8:45 AM UTC
Question

Unable to install the bundles...

VS Code report: "Unable to contact the STM32Cube registry, verify your Internet connection..."

Can I know the registry URL of the STM32Cube bundles registry and test its connection?

wechat_2025-08-29_164253_806.png

wechat_2025-08-29_164326_927.png

This topic has been closed for replies.

25 replies

Nawres GHARBI
ST Technical Moderator
Sep 1, 2025 7:54 AM UTC

Hi @emiya0306 

If you are hidden behind your company security, you probably need to configure a proxy and certificate to be able to access servers and download packages

This is how you will succeed in having full server access with our STM32Cube extension for VSCode.

 

How to Configure the proxy:

  • Open settings and type proxy in the search bar

NawresGHARBI_0-1756713156797.png

 

NawresGHARBI_2-1756713156809.png
NawresGHARBI_3-1756713156812.png

NawresGHARBI_4-1756713156815.png

 

Put your proxy in this format http://user:pass@Proxy-address:port

How to Configure the certificate:

  • Assuming your corporate self signed cert is trusted by your OS, you can now configure VS Code to use the OS cert. Launch VS Code, go to File > Preferences > Settings > Search for "certificates" and check the box for Http > Experimental: System Certificates V2 ".
    IT Controls whether experimental loading of CA certificates from the OS should be enabled

  • Otherwise make sure that the certificates are imported into your OS and trusted in system category. Then, go into VSCode settings, Application, Proxy, and UNCHECK the "System certificates" option. Restart VSCode and RE-CHECK it. Restart again, and it works.
  • if you want to do it the Manual way
  1. Open a corporate portal home page in browser and download Root CA certificate. This certificate is usually the first one in the hierarchy of 3 certificates available there. Another option is to ask security team to provide you a corporate Root CA certificate file in Base-64 format.
  2. Right-click the certificate file and select Install Certificate.
  3. Add Windows Environment variable NODE_EXTRA_CA_CERTS with path to this certificate file.
  4. Restart Visual Studio Code and try again.
emiya0306Author
Associate
Sep 12, 2025 11:36 AM UTC

Hi @Nawres GHARBI 

I think I don't have any company security, and just install STM32Cube for VSCode at home.

Julien D
ST Employee
Sep 12, 2025 12:09 PM UTC

Hi @emiya0306,

There is an error in the output shown in one of your screenshot, but partially visible because of vscode notifications.

Could you open a vscode terminal, execute the command cube bundle list-online, and paste here the error if any ?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Julien D
ST Employee
Sep 17, 2025 6:54 AM UTC

Everything looks ok from the logs, the failures are due to the fact that our underlying cube command fails to get the list of remote bundles, we have an internal discussion about your case on-going.

In the meantime, you can retry after removing every stm32cube folders:

  • C:\Users\41541\AppData\Local\stm32cube
  • C:\Users\41541\AppData\Roaming\stm32cube
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
emiya0306Author
Associate
Sep 17, 2025 11:09 AM UTC

Thanks a lot, I retry the method and it seems not work.

And, if you need more information, please feel free to contact me. ;)

ST Employee
Sep 17, 2025 1:16 PM UTC

Hi,

Could you help us investigate two things, we are a bit suspicious that Your user name could be interpreted wrongly. 

Do you have this as a login name 41541 ?

Can you run  echo $LASTEXITCODE after running cube --verbose bundle list-all-online

 

emiya0306Author
Associate
Sep 17, 2025 11:15 PM UTC

Hi @Niklas-Dahlquist ,

"41541" is my Microsoft Email Account, the full name is "41541xxxx@xx.xxx". I run "whoami" in PowerShell, it show "laptop-2n9slqe6\41541".

It works on echo $LASTEXITCODE and cube --verbose bundle list-all-online. 

wechat_2025-09-18_070658_137.png

But if I run STM32Cube: Install prerequisite bundles, it show these reports.

wechat_2025-09-18_071304_820.png

Julien D
ST Employee
Sep 18, 2025 1:22 PM UTC

Seems like you are now able to list the content of the bundle registry, did you changed something (network connection, etc..) on your side which could explain?

What Niklas suggested was to do the echo $LASTEXITCODE once the cube command completes. It allows to print the exit code of the last executed command (usually 0 means success, >0 means a failure).

The second screenshot highlights that there are still some issues with the installation of the required bundles. Could you run the following commands in the suggested order?

cube bundle list
echo $LASTEXITCODE
cube bundle install cube-code-manifest@1.0.3+st.1 --yes
echo $LASTEXITCODE
cube bundle install cmake ninja --yes
echo $LASTEXITCODE
cube bundle list
echo $LASTEXITCODE

 

list: lists the bundles installed on your PC.

--yes: accepts the bundle licences by default (up to you to remove this option to read the licence terms)

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Julien D
ST Employee
Sep 18, 2025 3:20 PM UTC

Just sent a PM

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
chaaalyy
Senior II
Sep 24, 2025 6:25 PM UTC

Also here: Came back to ST after a (very long) while because the VScode-approach made me curious. But what did i expect after all the experiences from earlier years, even the (everywhere recommended and advertised by ST´s newsletter...) try to install the preview version of the STM32cube extensions failed immediately... Fortunately i didn´t try this on a production machine and used a dedicated testrig...
Just as a hint for the extension-developers: Check your filesizes and SHA256 checksums ;)
I for myself uninstalled everything and don´t waste more time on that early alpha-stage package.


Julien D
ST Employee
Sep 24, 2025 7:49 PM UTC

Thanks @chaaalyy for sharing your experience here and there.

To be exact what you face is likely unrelated to this topic; the bundle registry is currently down, our ISP is working on it. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Julien D
ST Employee
Sep 25, 2025 6:59 AM UTC

@chaaalyy @Jakob K. The bundle registry service is now online, let us know if something continues to fail. Otherwise apologize for bad experience, the first time it happened with this server location since 2019.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Jakob K.
Associate
Oct 4, 2025 4:57 PM UTC

Hi @Julien D. Eventually it worked, seems I chose an unlucky date to try the Cube extensions :( 

Now I am experiencing the  'Unhandled: on_readmemory_request not available in PyDevJsonCommandProcessor' message and VS Code's Python Debugger no longer works. The issue has been reported here and there. Can you explain what happens using the ST extensions and is using VS Code profiles the only possible solution?

Julien D
ST Employee
Oct 5, 2025 7:51 PM UTC

@Jakob K. I can’t write more about, excepting that we have an internal ticket for this specific issue. Hopefully we’ll deliver a fix in a next release if something is feasible on our side. 

Until then Profiles are the way to go yes. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Julien D
ST Employee
Oct 7, 2025 2:21 PM UTC

@Jakob K. The 'Unhandled: on_readmemory_request not available in PyDevJsonCommandProcessor'  has been analyzed and fixed, it will be delivered with next release. Apologize for the inconvenience.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.