Skip to main content
KnarfB
Super User
Jul 13, 2024 6:55 AM UTC
Question

STM32 VS Code Extension generates startup file with unusable g_pfnVectors

Using STM32 VS Code Extension 2.0.1 to create empty project for STM32C0116-DK board.

The generated startup_stm32c011f6ux.s file contains handlers in wrong (alphabetic ???) order:

 

 

 

g_pfnVectors:
 .word	_estack
 .word	Reset_Handler
 .word	NMI_Handler
 .word	HardFault_Handler
 .word	0
 .word	0
 .word	0
 .word	0
 .word	0
 .word	0
 .word	0
 .word	SVC_Handler
 .word	0
 .word	0
 .word	PendSV_Handler
 .word	SysTick_Handler
 .word	ADC_IRQHandler 			/* ADC interrupt */
 .word	DMA1_Channel1_IRQHandler 			/* DMA1 channel 1 interrupt */
 .word	DMA1_Channel2_3_IRQHandler 			/* DMA1 channel 2 and 3 interrupts */
 .word	DMAMUX_IRQHandler 			/* DMAMUX interrupts */
 .word	EXTI0_1_IRQHandler 			/* EXTI line 0 and 1 interrupt */
 .word	EXTI2_3_IRQHandler 			/* EXTI line 2 and 3 interrupt */
 .word	EXTI4_5_IRQHandler 			/* EXTI line 4 and 5 interrupt */
 .word	I2C_IRQHandler 			/* global interrupt (combined with EXTI 23) */
 .word	RCC_IRQHandler 			/* RCC global interrupt */
 .word	RTC_IRQHandler 			/* RTC interrupts (EXTI lines 19) */
 .word	SPI_IRQHandler 			/* SPI/I2S global interrupt */
 .word	TIM1_BRK_UP_TRG_COM_IRQHandler			/* TIM1 break, update, trigger and commutation interrupts */
 .word	TIM1_CC_IRQHandler 			/* TIM1 Capture Compare interrupt */
 .word	TIM3_IRQHandler 			/* TIM3 gloabal interrupt */
 .word	TIM14_IRQHandler 			/* TIM14 gloabal interrupt */
 .word	TIM16_IRQHandler 			/* TIM16 global interrupt */
 .word	TIM17_IRQHandler 			/* TIM17 global interrupt */
 .word	USART1_IRQHandler 			/* USART1 global interrupt (combined with EXTI 25) */
 .word	USART2_IRQHandler 			/* USART2 global interrupt (combined with EXTI 25) */
 .word	WWDG_IRQHandler 			/* Window watchdog interrupt */
 .size g_pfnVectors, .-g_pfnVectors

 

 

 

wheras CubeMX 6.12 generates the correct one:

 

 

 

g_pfnVectors:
 .word _estack
 .word Reset_Handler
 .word NMI_Handler
 .word HardFault_Handler
 .word 0
 .word 0
 .word 0
 .word 0
 .word 0
 .word 0
 .word 0
 .word SVC_Handler
 .word 0
 .word 0
 .word PendSV_Handler
 .word SysTick_Handler
 .word WWDG_IRQHandler /* Window WatchDog */
 .word 0 /* reserved */
 .word RTC_IRQHandler /* RTC through the EXTI line */
 .word FLASH_IRQHandler /* FLASH */
 .word RCC_IRQHandler /* RCC */
 .word EXTI0_1_IRQHandler /* EXTI Line 0 and 1 */
 .word EXTI2_3_IRQHandler /* EXTI Line 2 and 3 */
 .word EXTI4_15_IRQHandler /* EXTI Line 4 to 15 */
 .word 0 /* reserved */
 .word DMA1_Channel1_IRQHandler /* DMA1 Channel 1 */
 .word DMA1_Channel2_3_IRQHandler /* DMA1 Channel 2 and Channel 3 */
 .word DMAMUX1_IRQHandler /* DMAMUX1 */
 .word ADC1_IRQHandler /* ADC1 */
 .word TIM1_BRK_UP_TRG_COM_IRQHandler /* TIM1 Break, Update, Trigger and Commutation */
 .word TIM1_CC_IRQHandler /* TIM1 Capture Compare */
 .word 0 /* reserved */
 .word TIM3_IRQHandler /* TIM3 */
 .word 0 /* reserved */
 .word 0 /* reserved */
 .word TIM14_IRQHandler /* TIM14 */
 .word 0 /* reserved */
 .word TIM16_IRQHandler /* TIM16 */
 .word TIM17_IRQHandler /* TIM17 */
 .word I2C1_IRQHandler /* I2C1 */
 .word 0 /* reserved */
 .word SPI1_IRQHandler /* SPI1 */
 .word 0 /* reserved */
 .word USART1_IRQHandler /* USART1 */
 .word USART2_IRQHandler /* USART2 */
 .word 0 /* reserved */
 .word 0 /* reserved */
 .word 0 /* reserved */

 .size g_pfnVectors, .-g_pfnVectors

 

 

 

please fix

KnarfB

This topic has been closed for replies.