Skip to main content
Associate II
Apr 22, 2026 2:44 PM UTC
Solved

Segger J-Link Setup for Full Chip Erase in VSCode

I'm using VSCode and J-Link for programming/flashing my STM23 MCUs.
Unfortunately using the default setup from SEGGER (https://kb.segger.com/J-Link_Visual_Studio_Code#Support),
J-Link only erases areas/pages needed.
I found no information about modifying the process of flashing.
Is there a way to modify the setup within VSCode in a way, to do a full chip erase when flasing by default?

Many thanks!

Florent V
Florent VBest answer
ST Employee
Apr 28, 2026 2:41 PM UTC

Hi @ETX,

You should be able to perform the full erase by adding this attribute to your debug configuration

"initCommands": ["monitor flash erase"],

 "initCommands" is the list of GDB commands sent after attaching to the target and before loading the image.

Kind Regards,

/Flo

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

5 replies

Pavel A.
Apr 22, 2026 4:13 PM UTC

Do you want to fully erase the STM32 every time you download a program, or only one time or rarely? If the latter, you can erase with the JFlash GUI or CLI, or other tool. Erasing only the needed pages actually is a good feature.

Andrew Neil
Super User
Apr 22, 2026 4:33 PM UTC

@Pavel A. wrote:

Erasing only the needed pages actually is a good feature.


Indeed it is!

 

@ETX You can also use STM32CubeProgrammer to do a full-chip erase.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ETXAuthor
Associate II
Apr 24, 2026 4:39 PM UTC

Yes, of course it's a good feature for standard applications.
But for developement purpose, where you are using eeprom emulation on separate flash pages, there would often be the need for a full chip erase.
And this shouldn't be done with a different software tool, it should work with VSCode developement enviroment.

So my question was about a way how to setup VSCode to do this automatically or maybe with a configuration modification of the J-Link debugger with J-Link Commander.
Till now, I couldn't find any information how to change the flashing behavior of the Segger driver.