Skip to main content
Associate
Feb 12, 2026 1:14 PM UTC
Question

Problem with setting up a project in VSCode with STm32 extension

piotrk_0-1770901809068.png

I get this type of error when I'm trying to setup a project with Nucleo-H563ZI and GCC here:

piotrk_1-1770901847779.png


I also get information that gdb is not running, while I've installed everything in the same way as I did on my previos laptop im my work. I've even changed system env for not checking tls or sha256 in stm but it still ain't working. Don't know what can I do.



10 replies

Nawres GHARBI
ST Technical Moderator
Feb 12, 2026 1:19 PM UTC

Hi @piotrk 

could you please try this command and show me the result

cube bundle list-online

piotrkAuthor
Associate
Feb 19, 2026 10:50 AM UTC

Hello, do You have any idea how to deal with such a problem with given information?

Cartu38 OpenDev
Graduate II
Feb 13, 2026 7:47 AM UTC

@piotrk 
Sounds like error reporting is explicit : you're facing downloading / network issues.

Close & restart VSCode. At startup STM32Cube is asking you license acceptance (notification on bottom right) prior executing some downloads. 
Having this happen at debug time means your current installation is partial what is not helping

piotrkAuthor
Associate
Feb 13, 2026 1:22 PM UTC

Hello @Nawres GHARBI so after i type that cube bundle list-online:
PS C:\PiotrK\test_proj\Proj_1_stm_test\test_3> cube bundle list-online
Name : Platform Version
---------------------------------------------------------------------
adoptium-jre : x86_64-windows ["17.0.16+8.st.1", "17.0.15+6.st.1", "17.0.14+7.st.6", "17.0.14+7.st.5"]
cmake : x86_64-windows ["4.0.1+st.3"]
cube-cmsis-scanner : x86_64-windows ["2.2.1", "1.1.3", "1.1.0", "1.0.1"]
cube-code-doc : all ["0.0.6+st.2", "0.0.5+st.1", "0.0.3+st.1", "0.0.2+st.1"]
cube-code-manifest : x86_64-windows ["1.0.9+st.2", "1.0.6+st.1", "1.0.3+st.1", "1.0.1+st.1", "1.0.0+st.1"]
cube-wrapper : x86_64-windows ["0.8.3", "0.7.3"]
gnu-gdb-for-stm32 : x86_64-windows ["14.3.1+st.2", "13.3.1+st.10", "13.3.1+st.9"]
gnu-tools-for-stm32 : x86_64-windows ["14.3.1+st.2", "13.3.1+st.9", "13.3.1+st.8"]
gnu-tools-for-stm32-13_3_1-description : all ["1.0.1+st.1", "1.0.0+st.1"]
gnu-tools-for-stm32-14_3_1-description : all ["1.0.1+st.1"]
jlink-gdbserver : x86_64-windows ["8.80.0+st.1", "8.38.0+st.1", "8.12.3+st.3"]
ninja : x86_64-windows ["1.13.1+st.1", "1.12.1+st.9"]
node : x86_64-windows ["20.19.4+st.1", "20.18.3+st.3"]
pack-manager : all ["0.3.12", "0.3.8", "0.3.7"]
pack-manager-snapshot : all ["2025.11.6", "2025.8.6", "2025.6.19", "2025.4.24"]
programmer : x86_64-windows ["2.21.0", "2.20.0", "2.19.0+st.1"]
rtos-proxy : x86_64-windows ["0.17.0+st.3"]
st-arm-clang : x86_64-windows ["19.1.6+st.10", "19.1.6+st.9", "19.1.6+st.8"]
st-arm-clang-19_1_6-description : all ["0.0.5+st.1", "0.0.4+st.1"]
st-arm-clang-hybrid : all ["19.1.6+st.3", "19.1.6+st.2"]
st-arm-clang-hybrid-19_1_6-description : all ["0.0.6+st.1", "0.0.5+st.1"]
st-arm-clangd : x86_64-windows ["19.1.2+st.3"]
stlink-gdbserver : x86_64-windows ["7.12.0+st.2", "7.11.0+st.1", "7.10.0+st.3"]
stlink-server : x86_64-windows ["2.1.1+st.7"]
stlink-upgrader : x86_64-windows ["3.16.9+st.4", "3.16.8+st.3"]
PS C:\PiotrK\test_proj\Proj_1_stm_test\test_3>

And answering to @Cartu38 OpenDev  I dont get any information about acceptance for VScode, but as I've written ive set environmet variables to do not check bundle checksum  allow STM bundles install and restarded computer and it still didn't work. But I will keep that in mind in case of getting that type of info in bottom right corner.
I only get this type of question:

piotrk_0-1770988859516.png

 

Cartu38 OpenDev
Graduate II
Feb 13, 2026 3:54 PM UTC

@piotrk 
So you're able to access to proper servers.

And you're getting expected notification asking you to agree about some extra material install.

If you accept it should solve your debug experience issue.

Cartu38OpenDev_0-1770998094794.png

 

piotrkAuthor
Associate
Feb 13, 2026 9:47 PM UTC

The first screen i posted here is the result i get when i click this Yes and i get errors such as the first photo I posted or this:

piotrk_0-1771019197183.png


If this would be so easy to just click yes i wouldn't post here, unfortunately it isn't ;(.

Cartu38 OpenDev
Graduate II
Feb 19, 2026 2:19 PM UTC

@piotrk i'm ready to help but i'm getting no feedback to my previous advices. Have you got a try and what are outcomes ?