Skip to main content
NSAUG.1
Associate III
Mar 4, 2026 12:13 PM UTC
Question

Memory Inspector does not resolve variable addresses

Hello,

 

In a paused debugging session, in the Run and Debug > Variables > Local list, if I right-click the varaible, the context menu has an item "Show in Memory Inspector".

Clicking it opens the Memory Inspector, but with the name of the variable as the adress ( &(pRxData) for example), which the memory viewer cannot resolve into the actual address (0x20003DC0 for example).

 

For this functionality to be most useful, I would expect either the Memory Inspector to be able to resolve the variable, or the command to open the Memory Inspector with the already-resolved address.

 

Best regards,

Nicolas

2 replies

Mikk Leini
Senior
Mar 5, 2026 7:39 AM UTC

I see the issue also, but only with some local stack based variables. Global and static variables work fine.

Using vscode with STM32Cube extensions v3.7.0, STLINK-V3MINIE and STM32N65x0 MCU. GCC compiler and -O2 optimization.

Nawres GHARBI
ST Technical Moderator
Mar 5, 2026 8:56 AM UTC

@NSAUG.1  thanks for reporting this issue ticket #3953  logged for fix