Skip to main content
allannick
Associate
Oct 18, 2023 1:12 PM UTC
Solved

meet “Unable to stat debugging. Debug server process failed to initialize” in VSC when debugging

I am trying to use STM32 VSC extension plugin on VSCode for a better coding experience, but error occored when I am trying to debugging.

allannick_0-1697633289766.png

VSCode suggested that build task finish successfully in the terminal.

It seems debugger failed to connect debug server. [I am not sure what debug server is and how they work. The only thing I know is that launch file has set up 2 tools named:

ST-LINK_gdbserver.exe and arm-none-eabi-gdb.exe. Iguess they are connected with each other and transmit debug info by TCP(?)]
 
I have already tried connect and reconnect my NUCLEO board on my computer. When debugger runnging, the stlink flashlight on the NUCLEO is blinking as normal (red-green-red-green). But somehow the program can't be uploaded. Also I've allowed the debugger access my network so the issue shouldn't caused by a block of my defender (I am using windows Defender only) on my computer.
 
But, however, the debugger crashed before everything I predicted happen and here is some related infos.
DEBUG CONSOLE output:
1: (76) LaunchOptions{"name":"Launch","type":"cppdbg","request":"launch","cwd":"D:\\Programs\\ENV\\STM32_plugged\\CUBER\\WIN_TS_IV\\TRY_V","program":"D:\\Programs\\ENV\\STM32_plugged\\CUBER\\WIN_TS_IV\\TRY_V\\build\\debug\\build\\TRY_V.elf","MIMode":"gdb","miDebuggerPath":"C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/arm-none-eabi-gdb.exe","miDebuggerServerAddress":"localhost:3333","debugServerPath":"C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_2.1.0.202305091550/tools/bin/ST-LINK_gdbserver.exe","debugServerArgs":"--stm32cubeprogrammer-path C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.0.202305091550/tools/bin --swd --port-number 3333","serverStarted":"Waiting for connection on port .*//.//.//.","stopAtConnect":true,"postRemoteConnectCommands":[{"text":"load build/debug/build/TRY_V.elf"}],"logging":{"engineLogging":true},"preLaunchTask":"Build","__configurationTarget":6,"configSource":"workspaceFolder","debugType":"debug","__sessionId":"6cfcefe6-4251-4735-8b0e-188844f1368a"}
1: (140) Starting: "C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_2.1.0.202305091550/tools/bin/ST-LINK_gdbserver.exe" --stm32cubeprogrammer-path C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.0.202305091550/tools/bin --swd --port-number 3333
1: (334) ->
1: (339) ->
1: (339) ->STMicroelectronics ST-LINK GDB server. Version 7.4.0
1: (340) ->Copyright (c) 2023, STMicroelectronics. All rights reserved.
1: (340) ->
1: (340) ->Starting server with the following options:
1: (340) -> Persistent Mode : Disabled
1: (340) -> Logging Level : 31
1: (340) -> Listen Port Number : 3333
1: (340) -> Status Refresh Delay : 15s
1: (340) -> Verbose Mode : Disabled
1: (341) -> SWD Debug : Enabled
1: (341) ->
1: (346) ->COM frequency = 4000 kHz
1: (347) ->Target connection mode: Default
1: (353) ->Reading ROM table for AP 0 @0xe00fffd0
1: (356) ->Hardware watchpoint supported by the target
1: (359) ->ST-LINK Firmware version : V2J42M27
1: (360) ->Device ID: 0x410
1: (360) ->PC: 0x8000d10
1: (360) ->ST-LINK device status: HALT_MODE
1: (360) ->ST-LINK detects target voltage = 3.26 V
1: (361) ->ST-LINK device status: HALT_MODE
1: (361) ->ST-LINK device initialization OK
1: (361) ->Stm32Device, pollAndNotify running...
1: (363) ->SwvSrv state change: 0 -> 1
1: (364) ->Waiting for debugger connection...
1: (364) ->Waiting for connection on port 3333...
1: (364) ->Waiting for connection on port 3334...
1: (10323) <-logout
1: (10339) Send Event AD7MessageEvent

This is my "launch.json" file:

{
  "version": "0.2.0",
  "configurations": [
   
    {
      "name": "Launch",
      "type": "cppdbg",
      "request": "launch",
      "cwd": "${workspaceFolder}",
      "program": "${command:cmake.launchTargetPath}",
      "MIMode": "gdb",
      "miDebuggerPath": "C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/arm-none-eabi-gdb.exe",
      "miDebuggerServerAddress": "localhost:3333",
      "debugServerPath": "C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_2.1.0.202305091550/tools/bin/ST-LINK_gdbserver.exe",
      "debugServerArgs": "--stm32cubeprogrammer-path C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.0.202305091550/tools/bin --swd --port-number 3333",
      "serverStarted": "Waiting for connection on port .*//.//.//.",
      "stopAtConnect": true,
      "postRemoteConnectCommands": [
        {
          "text": "load build/debug/build/TRY_V.elf"
        }
      ],
      "logging": {
        "engineLogging": true
      },
      "preLaunchTask": "Build"
    }
  ]
}
This is my VSC layout:
allannick_1-1697634258592.png

 

As a freshman in STM32 development, I am not so familiar with the toolchain it use, hoping somebody could do me a favour. Sincerely.

 

This topic has been closed for replies.
allannick
allannickBest answer
Associate
Oct 22, 2023 7:42 AM UTC

Laterly, I founded a tips by browsing the overview page of STM32 VS Code Extensions on VSC Market place which says: When starting the debugger it can happen the connection to the board fails with a Visual Studio Code message reporting "Unable to start debugging. No process is associated with this object."
The root cause can be identified in the DEBUG CONSOLE. Most probably the following message is reported: "Error in initializing ST-LINK device. Reason: ST-LINK firmware upgrade required." 

    Then I tried to update my stlink firmware by "CubeProgrammer", and everything in vscode are running normally now. 

1 reply

allannick
allannickAuthorBest answer
Associate
Oct 22, 2023 7:42 AM UTC

Laterly, I founded a tips by browsing the overview page of STM32 VS Code Extensions on VSC Market place which says: When starting the debugger it can happen the connection to the board fails with a Visual Studio Code message reporting "Unable to start debugging. No process is associated with this object."
The root cause can be identified in the DEBUG CONSOLE. Most probably the following message is reported: "Error in initializing ST-LINK device. Reason: ST-LINK firmware upgrade required." 

    Then I tried to update my stlink firmware by "CubeProgrammer", and everything in vscode are running normally now.