Skip to main content
Associate
Feb 25, 2026 1:43 PM UTC
Solved

how to view debug variables in hex (VSCode with STM32CubeIDE extension)

There does not seem to be any way of viewing a debug variable in hex.
The closest workaround is to prefix (void*) before the expression in the watch window. 
This is no good for viewing an array of hex digits like for example a CAN bus message.

Florent V
Florent VBest answer
ST Employee
Feb 25, 2026 9:15 PM UTC

Hi @Michael_John

You can add the following attribute to your debug configuration:

"preRunCommands": [
 "set output 16"
],

 

Best Regards,
/Flo

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

6 replies

Florent V
Florent VBest answer
ST Employee
Feb 25, 2026 9:15 PM UTC

Hi @Michael_John

You can add the following attribute to your debug configuration:

"preRunCommands": [
 "set output 16"
],

 

Best Regards,
/Flo

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
Feb 26, 2026 4:22 PM UTC

Hi Forent
Thank you, that works nicely.
I see you have already marked your own answer as accepted.
Thank you for your response

Explorer
Apr 19, 2026 4:21 PM UTC

Worked! Thanks!!

Associate
May 12, 2026 5:48 AM UTC

I was using watch variable via STM32 Run and Debug and found I could not use ,h or ,x or maybe ,b to display number in hex or binary. If we to adopt Visual Code (away from STM32 CubeIDE), why it is not supported for very fundamental debug tools?. Is there plan to fix this for upgrade STM32 package in extension?

 

Cartu38 OpenDev
Graduate II
May 12, 2026 6:06 AM UTC

@Riscy24 

Current trick shared by @Florent V already.

Shared already as part of roadmap: any update here ?

Not supported today because variables view is VS Code native i guess.

MWils.4
Associate
Jul 15, 2026 8:32 PM UTC

To flesh out this answer, the text above goes in .vscode\launch.json

I put the new entry after the “name’: entry.

My launch.json has 3 configurations, so I added the text in all three. 

This feature should be MUCH easier to find, but maybe I don’t know where to look. Is there a setup guide for the STM32 VSCode plugins?