Skip to main content
Associate
November 6, 2025
Question

How to Just download without starting a debug session?

  • November 6, 2025
  • 4 replies
  • 696 views

How can I use VS Code to download only the firmware? I can do it using debug mode, but I don't want to trigger debug. Is it possible to run it automatically after downloading, like CubePRG? I'm not very familiar with CMake. Thank you.

-----------------------------------------------------------------

Erasing internal memory sectors [0 6]
Download in Progress:
2
File download complete
Time elapsed during download operation: 00:00:06.418
-------------------------------------------------------------------
Just take out this part separately

4 replies

Ethan HUANG
ST Employee
November 6, 2025

One of the options is using "task" as shown below:

EthanHUANG_0-1762404271900.png

  1. Unzip the attached zip to get the file tasks.json.
  2. Assign the paths in the file tasks.json based on your environment.
  3. Put tasks.json into folder .vscode in your project
  4. Press "Ctrl+Shift+P" to bring up Command Palette and choose "Tasks: Run Task" as shown in the picture above, and then select "Flash STM32 (CubeProgrammer)" which is assigned in the tasks.json.

 

TravelCatAuthor
Associate
November 6, 2025

Thank you very much, it works very well. Have you considered integrating it into an extension in the future? I feel it would be very useful.

Ethan HUANG
ST Employee
November 6, 2025

This is also in my wish list.

 

TravelCatAuthor
Associate
November 6, 2025

iヾ(≧▽≦*)o I am looking forward to the update going live.