Skip to main content
Associate
Sep 18, 2025 7:26 AM UTC
Question

Header files not found by VSC

I have problem that most headers are not visible so a lot of dependent problems occured.

All files are present - the same project compoiled in STM32CubeIDE works.

There is note that "clang(pp_file_not_found)"

Tried to add paths in CMakeLists.txt but no luck.

4 replies

Cartu38 OpenDev
Graduate II
Sep 18, 2025 8:55 AM UTC

@Jacek3 have you a .clangd file added by STM32Cube to your project root ?

If not maybe look at https://community.st.com/t5/stm32cube-for-visual-studio-code/after-installing-stm32cube-for-visual-studio-code-why-do-two/td-p/839930 ... not code indexing related by explain a bit proper process to end up good setup.

Jacek3Author
Associate
Sep 19, 2025 8:04 AM UTC

@Cartu38 OpenDev Thank You for response.

Yes, I have .clangd file, but it was created rather by VSC, not STM32Cube.

My .clangd file:

CompileFlags:
 Add:
 - '-ferror-limit=0'
 - '-Wno-implicit-int'
 CompilationDatabase: build/release/build
Diagnostics:
 Suppress:
 - unused-includes
 - unknown_typename
 - unknown_typename_suggest
 - typename_requires_specqual

 

I have in Output window:

[driver] NOTE: You are configuring with preset release, but there are some overrides being applied from your VS Code settings.
and
can't open .map file
 
I suppose that the reason is that STM32Cube use .../Release or .../Debug while compile but VSC use .../buil/release or .../built/debug. 
Do You know how can i change it in VSC?
Cartu38 OpenDev
Graduate II
Nov 22, 2025 8:02 AM UTC

@Jacek3 
Cartu38OpenDev_0-1763798512083.png

 

Visitor II
Nov 19, 2025 5:26 PM UTC

I don't think the debug and release thing is the issue, I'm on Debug and have the same issue, and to change it just go to Command Palette: (Ctrl:Shift:P) and then type CMake: Select Configure Preset and select that