Skip to main content
dze.1
Associate II
Jun 27, 2025 1:42 PM UTC
Solved

Debugging under VS Code failed

Hi,

I followed exactly the instructions of ST's youtube tutorial "Get started with STM32Cube for VS Code: from installation to debugging". (https://www.youtube.com/watch?v=aWMni01XGeI)

Everything went perfect, the demo builds without problems.

When it comes to debugging, VS Code gives me the error "Failed to install missing pack. "STMicroelectronics.stm32u3xx_dfp.1.0.0"

Additional the is the same error as extension notification, see below.

I tried Ctrl+Shift+P + Restore STM32Cube CMake projects configuration, but to no avail.

Same thing happens with other STM32 CMake projects.

What did I miss?

 

Thank You in advance

This topic has been closed for replies.
Julien D
Julien DBest answer
ST Employee
Jun 30, 2025 3:37 PM UTC

Looks like you have a custom openssl install in c:\ws\deps\openssl

If this install is required for something else you may need to set its openssl.cnf to

openssl_conf = openssl_init

[openssl_init]
ssl_conf = ssl_sect

[ssl_sect]
system_default = system_default_sect

[system_default_sect]
Options = UnsafeLegacyRenegotiation

 I can't try this on my side though.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

10 replies

Julien D
ST Employee
Jun 27, 2025 1:47 PM UTC

Hi @dze.1,

You can try to install manually the missing pack from vscode terminal with the command cube pack install STMicroelectronics.stm32u3xx_dfp.1.0.0 and check if there is any relevant error.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
dze.1
dze.1Author
Associate II
Jun 27, 2025 3:00 PM UTC

Hi,

thanks for reply.

I should mention I'm using STM32Cube for Visual Studio Code 3.4.11 as recommended in the tutorial.

Neither cube pack install STMicroelectronics.stm32u3xx_dfp.1.0.0 nor STM32Cube: pack install STMicroelectronics.stm32u3xx_dfp.1.0.0 succeeded.

Such a command seems not to exist. I have attached all other available STM32 extension commands below.

But STM32Cube: Synchronize pack list runs without error. But again to no avail.

Thanks.

2025-06-27 16_45_24-VS_Example - Visual Studio Code3.jpg

 

 

 

 

KnarfB
Super User
Jun 27, 2025 4:05 PM UTC

This command is to be entered in the terminal, not in the command palette:

KnarfB_0-1751040208985.png

hth

KnarfB

Julien D
Julien DBest answer
ST Employee
Jun 30, 2025 3:37 PM UTC

Looks like you have a custom openssl install in c:\ws\deps\openssl

If this install is required for something else you may need to set its openssl.cnf to

openssl_conf = openssl_init

[openssl_init]
ssl_conf = ssl_sect

[ssl_sect]
system_default = system_default_sect

[system_default_sect]
Options = UnsafeLegacyRenegotiation

 I can't try this on my side though.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
dze.1
dze.1Author
Associate II
Jul 2, 2025 10:19 AM UTC

Hallo Julien,

I have no openssl installed.

However, I did complain to my company IT again. They solved the problem now. Some server side internal IT stuff I have no insight to. Now it works.

Thank you very much for your help and patience.

Dirk

Julien D
ST Employee
Jul 2, 2025 11:12 AM UTC

Great!

Thanks for your feedback.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.