Skip to main content
LordN
Associate II
Apr 2, 2026 2:04 PM UTC
Question

Debugging often hangs (infinite loop of "Read 4 bytes @ address ...")

Hello,

I've been working with the new VS Code extensions for several weeks, and debugging feels quite unstable. I'm using a j-Link Plus. At random times, I suddenly can't debug anymore, everything seems to freeze, and in the Debug Console I see something like this:

debug hang.png

The number (6760 here) increases by hundreds per second and will never stop. Every time such a random debug freeze happens, I see this last line with the counting number box, always reading 4 bytes somewhere (different addresses), as if some read action hangs in an endless loop. Only way to get it working again is by closing the whole debug session and starting anew.

Sometimes I can debug for an hour without this issue, sometimes I get this every few minutes. It's not related to some code position, happens in different debug configurations (flash / attach to running), happens in different projects, with different (or no) watched variables, on different PCBs, with different cables to the debug probe, with different clang optimization levels. Restarting VS Code and reconnecting the probe USB cable don't seem to help much either. I see no systematic trigger at all.

Today I've updated jlink-gdbserver to 9.14.1+st1, but the issue continues.

Using the same probe and same ELF in SEGGER Ozone works without any such problem, have been using this probe and Ozone for years. So it must be something in VS Code or the GDB extensions.

My launch config is this:

{
	"name": "Build & Debug App (j-Link)",
	"type": "jlinkgdbtarget",
	"request": "launch",
	"origin": "snippet",
	"cwd": "${workspaceFolder}",
	"presentation": {
		"group": "j-Link",
		"order": 1
	},
	"preLaunchTask": "Build App",
	"imagesAndSymbols": [
		{
			"imageFileName": "${workspaceFolder}/build/Debug/APPLICATION.elf"
		}
	],
	"deviceName": "STM32H743II",
	"deviceCore": "Cortex-M7",
},

Any idea what could be the issue?

(I also tried an ST-Link for debugging, but that one has different problems like sometimes being extreeeemely slow, so it's not a good alternative either.)

7 replies

Nawres GHARBI
ST Technical Moderator
Apr 3, 2026 8:01 AM UTC

hi @LordN 

is it reproducible with all your projects or a project in particular, if yes please attach an example 

LordN
LordNAuthor
Associate II
Apr 7, 2026 11:53 AM UTC

Hello,

This has happened in multiple projects. They all have a very similar setup though. What files do you need to see? I think I'm not allowed to share the whole software here...

Nawres GHARBI
ST Technical Moderator
Apr 7, 2026 11:59 AM UTC

Hi @LordN 

you can share by message, if your SW is confidential you can create a basic example reproducing the issue

LordN
LordNAuthor
Associate II
Apr 16, 2026 1:16 PM UTC

Some days ago, I plugged the j-Link USB directly into a USB port on my laptop instead of via a USB hub (where it's been for years), and since then I have not encountered this problem anymore so far.

So the issue probably lies somewhere on the USB communication level which sometimes gets corrupted due to some other USB device on the same hub?? This is not easily reproducable or debuggable...

If anyone sees similar issues, just try to plug the probe somewhere else.

Ozone
Principal
Apr 16, 2026 1:34 PM UTC

> If anyone sees similar issues, ...

Different attached USB devices and different application(s), but most often with an USB2.0 hub.

I suppose you speak about Windows, specifically Win11.

SilentButeo2
Associate
Jun 10, 2026 9:09 AM UTC

Since a few weeks we also see this behaviour. We have a STM32F427VI system. Probably also started by some kind of update, because we didn’t had it before and older FW build now also have this behaviour.
jlink-gdbserver 9.24.0+st.1 (latest)

 

2 observations we currently have:

  1. using build option Og seems to stop triggering the issue (previous we had O0).
  2. currently using O0, but with nothing in the watch of VS code also seems to stop triggering the issue.

Putting the j-link direct to the PC, does not stop triggering the issue.

 

I first had an ST-link. There I also encountered problems during debug. But in those cases, I could see no feedback in the VSC UI. Just the debugger that “hangs”. Then switched to the j-link where we had the running number UI feedback of the problem.