Skip to main content
Visitor II
Feb 8, 2025 2:17 PM UTC
Question

Compiling an OLED Display with SSD1306 and Fonts in VS Code

I am testing a very simple OLED display using the SSD1306 driver and fonts, referring to the link below. However, the code does not compile successfully.

Are there any possible reasons for this issue?

スクリーンショット 2025-02-08 230949.png


/* USER CODE BEGIN Includes */
#include "fonts.h"
#include "ssd1306.h"
/* USER CODE END Includes */

/* USER CODE BEGIN 2 */
SSD1306_Init();
SSD1306_GotoXY (0,0);
SSD1306_Puts ("MICROPETA", &Font_11x18, 1);
SSD1306_GotoXY (0, 30);
SSD1306_Puts ("BY NIZAR", &Font_11x18, 1);
SSD1306_UpdateScreen();
HAL_Delay (1000);
SSD1306_ScrollRight(0,7);
HAL_Delay(3000);
SSD1306_ScrollLeft(0,7);
HAL_Delay(3000);
SSD1306_Stopscroll();
SSD1306_Clear();

int num=2024;
char snum[5];
SSD1306_GotoXY (30,20);
itoa(num, snum, 10);
SSD1306_Puts (snum, &Font_16x26, 1);
SSD1306_UpdateScreen();

//SSD1306_DrawLine(POINT1 X, POINT1 Y, POINT2 X, POINT2 Y, 1);
SSD1306_DrawLine(1,54,126,54,1);
SSD1306_UpdateScreen();
HAL_Delay (5000);
SSD1306_Clear();

// For Rectangle, we need to use two corner points
// SSD1306_DrawRectangle(POINT1 X, POINT1 Y, POINT2 X, POINT2 Y, 1);
SSD1306_DrawRectangle(17,1,115,14,1);
// SSD1306_DrawTriangle(POINT1X, POINT1Y, POINT2X, POINT2Y, POINT3X, POINT3Y, 1);
SSD1306_DrawTriangle(73,22,124,62,74,54,1);
// SSD1306_DrawCircle(CENTER POINT X, CENTER POINT Y, RADIUS, 1);
SSD1306_DrawCircle(34,50,13,1);
SSD1306_UpdateScreen();
/* USER CODE END 2 */

This topic has been closed for replies.

2 replies

Andrew Neil
Super User
Feb 8, 2025 3:22 PM UTC

@kaakun wrote:

Are there any possible reasons for this issue?


The reason is as stated in the messages - you have undefined references!

That means you have called those functions, but you have not defined them.

  • Did you omit to include some  .c source file(s) which define(s) them?
  • Did you omit to include some pre-compiled binary file (eg, a library) which defines them?
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
Feb 8, 2025 4:01 PM UTC

Attach all of Build log, look at the FIRST errors

Looks not to be compiling ssd1306.c as linker is complaining the body code it's trying to bind against is missing.

Is it perhaps compiling one of the files as .cpp / C++

The source code you attached looks to be building, so probably not that.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..