Skip to main content
Associate
May 4, 2026 4:23 PM UTC
Question

Clangd preprocessor define issue - opacity stops working after toggling Configure

Hello,

I'm having an issue for a few latest versions of clangd. I was hoping this issue would be resolved in newest update of VS Code extension - clangd v1.0.5., but still with no success. 

Issue: I'm using two Configurations in CMake -> Configure. Configurations are defined in CMakePresets.json like this:

Michael12_0-1777910694573.png

I'm using define as this:

Michael12_1-1777910755529.png 

I'm switching configuration via CMake->Configure->Select Configure Preset.

Now, switching Configuration on clangd v1.0.2 will highlight/fade non-used define correctly. Switching to clangd version v1.0.4, it's no longer working correctly.

I have set the setting on v1.0.4 as such:

Michael12_2-1777911369689.png

Opacity is 0.5. If I change the Configuration, the Opacity no longer works on the code segment:

Michael12_3-1777911440952.png

But, if I go to settings and just enter the value 0.5, it starts working again, untill the next Configure change.

This issue in not on v1.0.2, only at v1.0.4 and v1.0.5.

4 replies

Cartu38 OpenDev
Graduate II
May 4, 2026 8:14 PM UTC

@Michael12 
What happens if after preset selection update you're closing & opening back your .c file ? Is opacity applied in sync. expectation ?

Cartu38 OpenDev
Graduate II
May 4, 2026 8:27 PM UTC

@Michael12 
I'm able to face the same starting 1.0.4. File closure or switch between 2 editor tabs is applying proper rendering refresh.

Michael12Author
Associate
May 5, 2026 7:02 AM UTC

Yes! You're right. Switching tabs or closing and reopening the file will refresh the opacity. It's still little inconvenient. Is it possible to fix it in future? Thanks for help.

Kouthair
ST Technical Moderator
May 5, 2026 4:09 PM UTC

Hello @Michael12 ,

I was able to recreate the same behavior, and I have forwarded your request to our development team to look further into it. (Internal ticket ID: 0062377)

I will let you know if there are any updates on this matter.
As previously discussed, switching tabs does set the correct opacity.

PS: Ticket ID: 0062377 is an internal tracking number and is not accessible or usable by customers.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.