Skip to main content
Associate II
Mar 13, 2026 2:51 AM UTC
Question

bundles manager takes very long time to load

Hi, the extension version is 3.8.0, and it usually takes 5min to load, is that normal? Also, is there any CDN or dedicated server for Chinese users? cuz it's troublesome to download those bundles here. Thx

17 replies

Julien D
ST Employee
Mar 13, 2026 7:07 AM UTC

Hi @ianzone,

Yes Chineses users have their regional server, and nothing changed in term of infrastructure with the release of version 3.8.0. Means maybe a tooling issue.

How long take the 2 following commands aiming to list the remote and local bundles?

cube bundle list-online
cube bundle list

It should somehow reply immediately for both.

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ianzoneAuthor
Associate II
Mar 19, 2026 1:18 AM UTC

Seems not a server issue, those 2 commands replied immediately, but the extension still takes long time to load. 

屏幕截图 2026-03-19 091754.png

Julien D
ST Employee
Mar 31, 2026 6:45 AM UTC

Hi @ianzone,

Thanks for sharing the logs, indeed it highlights what could look like really bad network performance.

First I see that you use a local proxy, do you have the capability to make some test without it?

It would be interesting to compare bundle downloads speeds in the 2 configurations (with and without your proxy) by manually installing a toolchain bundle: 

cube bundle install gnu-tools-for-stm32@^13.0.0

Screenshot 2026-03-31 at 08.39.15.png

It can be removed later thanks this command:

cube bundle remove gnu-tools-for-stm32@^13.0.0

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ianzoneAuthor
Associate II
Apr 1, 2026 2:45 AM UTC

Without proxy: 7000 KB/s

With proxy: timeout

I've put *st.com into the proxy whitelist; it shouldn't affect the download speed. 

Julien D
ST Employee
Apr 1, 2026 8:50 AM UTC

Wouldn't this clearly indicate that your local proxy configuration is somehow blocking traffic? If so, your proxy logs should help identify which flow is being rejected.

Additionally, if your proxy performs SSL inspection, you may need to set the NODE_EXTRA_CA_CERTS variable to configure your proxy's root CA certificate. A simple cube pack sync command will show SSL errors if the handshake fails. If the command works, you can ignore this comment.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ianzoneAuthor
Associate II
Apr 24, 2026 2:55 AM UTC

sometimes it fails

2026-04-24 10:44:10.437 [Info]  Adding STM32Cube CLI path to environment: c:\Users\yihen\.vscode\extensions\stmicroelectronics.stm32cube-ide-core-1.2.1-win32-x64\resources\binaries\win32\x86_64
2026-04-24 10:44:10.559 [Info]  Configuring CUBE_BUNDLE_PATH environment: C:\Users\yihen\AppData\Local\stm32cube\bundles
2026-04-24 10:44:10.560 [Info]  NODE_EXTRA_CA_CERTS is not set
2026-04-24 10:44:10.650 [Info]  CMSIS_PACK_ROOT=C:\Users\yihen\AppData\Local\stm32cube\packs
2026-04-24 10:44:15.379 [Info]  cube wrapper version: 0.10.2
2026-04-24 10:44:16.317 [Info]  Online bundle cache built
2026-04-24 10:51:17.893 [Info]  Installing STM32Cube bundles prerequisites
2026-04-24 10:52:16.145 [Error]  Failed to initialize STM32Cube bundles: Failed to get list of available updates. Command failed with
2026-04-24 10:52:16.150 [Info]  STM32Cube Core activated (485736ms)
2026-04-24 10:52:16.152 [Info]  Syncing CMSIS-Pack metadata for C:\Users\yihen\AppData\Local\stm32cube\packs
2026-04-24 10:52:16.154 [Info]  No need to sync metadata, since recently updated.
ianzoneAuthor
Associate II
Apr 30, 2026 1:29 AM UTC

I suspect this extension downloaded the toolchain everytimes, even if there were local files

ianzone_0-1777512548348.png

 

Julien D
ST Employee
Apr 30, 2026 7:22 AM UTC

Hi @ianzone,

 


I suspect this extension downloaded the toolchain everytimes, even if there were local files

 

Be assured, it is not downloaded every time. However, yes, when registering a bundle in a project, network access may be used to get an updated list of bundles in the local metadata cache.

I see 2 errors:

[Error]  Failed to initialize STM32Cube bundles: Failed to get list of available updates.

Likely, the cube bundle list-online command run by the extension at startup failed, while a couple of days ago you said it worked fine. Was there any network change in the meantime?

The screenshot notification.

Do you already have any .settings/bundle.store.json file in your project?

If so does it contain Ninja?

Maybe try to do the same operation from the CLI to ensure no useful error message is being hidden by the UI: cube --cwd <project_path> bundle install ninja --project

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ianzoneAuthor
Associate II
May 7, 2026 12:45 AM UTC

Hi, I couldn't find any bundle.store.json in my computer. is that the case? and how can i get it?