Skip to main content
AHugh.2
Associate III
Aug 6, 2025 9:53 AM UTC
Solved

Add reset MCU command to debug toolbar

Hi,

Is it possible to add a MCU reset command to the debug toolbar? I.e. a button that does a pause then "monitor reset" type sequence? Of course I can do this manually in the debug console, but it'd be nice to have a button to do it, to complement the full restart button.

Thanks!

Nawres GHARBI
Nawres GHARBIBest answer
ST Technical Moderator
Aug 19, 2025 8:18 AM UTC

Thanks @AHugh.2   for the proposal

Ticket created for this change request 

14 replies

TDK
Aug 6, 2025 1:21 PM UTC

This one doesn't work? What is a monitor reset type sequence?

TDK_0-1754486453015.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
AHugh.2
AHugh.2Author
Associate III
Aug 6, 2025 4:16 PM UTC

Thanks, but I am referring to Cube integration in VSCode not CubeIDE.

"monitor reset" is a command you give to GDB to tell it to reset the target, without it going through the reconnect, and flashing the image again.

 

Nawres GHARBI
Nawres GHARBIBest answer
ST Technical Moderator
Aug 19, 2025 8:18 AM UTC

Thanks @AHugh.2   for the proposal

Ticket created for this change request 

ADunc.1
Senior
Nov 5, 2025 8:53 PM UTC

Yup, definitely need that reset button.  In my case I use a bootloader.  Debugging programs just the application.  But cant properly run the application with it going through the bootloader first.  So, need to be able to reset after programming to force the bootloader to be executed.

And besides, every debugger I have ever used has a reset button so you can quickly start again with reprogramming (which takes forever on a full flash H7!).

ST Employee
Nov 6, 2025 7:14 AM UTC

@AHugh.2 
Thank you for reporting this issue.

I’m happy to share an early teaser with you: the reset feature is already part of our codebase, and we plan to deliver it as soon as possible. Stay tuned!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ozone
Principal
Nov 6, 2025 7:42 AM UTC

And I thought such a MCU reset command was standard ...

Ozone_0-1762414707779.png

Just saying ...

Florent V
ST Employee
Dec 15, 2025 4:44 PM UTC

Hi @AHugh.2 , @ADunc.1 and @Ozone ,

The reset button is officially available in the latest 3.7.0 release.

FlorentV_1-1765816985951.png

By default, it will execute :

  • monitor reset
  • tbreak <runEntry attribute value>
  • continue

However, you can customize these commands using the following attribute in your debug configuration

"quickReset": [
 "monitor reset",
 "tbreak main",
 "continue"
],


Kind Regards,
Flo

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ozone
Principal
Dec 16, 2025 7:17 AM UTC

As a remark ...

If the option "run to main" is disabled (i.e. the debugger should stop at the reset vector), a "reset MCU" should take that into account.

Florent V
ST Employee
Dec 16, 2025 8:24 AM UTC

Hi Ozone,

Thanks for the remark.

For info, without talking about "reset MCU" (aka "quickReset"), if the "runEntry" attribute is not set, then the program does not stop at startup. Otherwise, it would be blocking for users wanting to run their code.
In this case, it is easier to set the desired function in the "runEntry" attribute.

For the "quickReset", we chose to set a temporary breakpoint on the "runEntry" value or on "main" (if "runEntry" is not set). But again, it is entirely possible to customize this via the "quickReset" attribute.

And of course, if many agree with your remark, we can change our approach, no problem with that.

KR,
Flo

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Nawres GHARBI
ST Technical Moderator
Dec 16, 2025 8:29 AM UTC

available now 

AHugh.2
AHugh.2Author
Associate III
Dec 16, 2025 11:46 PM UTC

Hi,

One observation, say I want it just to reset and not break on main, then I have put this in the lauch.json:

"quickReset": [
 "monitor reset",
 "continue"
]

So just ommitted the "tbreak main" line, but I find doing this allows only one reset then no other debug commands seem to work - can't pause, and pressing the quick reset button again results in it the button becoming disabled and that's it.

With tbreak in, no problems.

Thanks.

 

Florent V
ST Employee
Dec 17, 2025 8:26 AM UTC

The error comes from a desynchronization between the GDB client and the VSCode debug session.
During the reset, the GDB client correctly sends the "continue" command after the reset.
However, VSCode does not synchronize, so any new command from VSCode is not handled by the GDB client.

In the meantime, to avoid this behavior with quickReset: [monitor reset; continue], you must at least set a manual breakpoint in the code so that the GDB client hits it and synchronizes with VSCode.

Note:

  • setting the breakpoint manually, rather than in the quickReset command, allows you to change the breakpoint before a reset.
  • if you are hung, setting the breakpoint after the reset will not work because the GDB client is running and will not respond.

 

BR,
Flo

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AHugh.2
AHugh.2Author
Associate III
Dec 17, 2025 2:35 PM UTC

Thanks for the response Florent.

In my case I was looking for a quick MCU reset and run to catch something with minimal "down-time". However it is not a big deal.