Skip to main content
mattias norlander
ST Technical Moderator
Oct 1, 2026 1:05 PM UTC

Introducing STM32CubeCLI: your STM32 toolchain from the command line

Related products:STM32 software tools

If you use STM32CubeIDE for Visual Studio Code, you have already used STM32CubeCLI.

Since April 2025 it has installed and updated the tools behind the extension, and since March 2026 it does the same for STM32CubeMX2. Now it is available on its own: one cube command to install, build, flash and debug from any terminal or CI runner, on Windows, Linux and macOS.

The idea is simple: your tools travel with your code.
 

What is STM32CubeCLI?

STM32CubeCLI brings together three things:

  • The `cube` command: one consistent way to call STM32Cube tools, such as cube cmake, cube programmer or cube stlink-gdbserver.
  • The bundle manager: installs, updates and pins tool versions from ST’s public online registry. No login, no hunting for downloads.
  • Bundles: the tools themselves: GCC, CMake, Ninja, STM32CubeProgrammer, ST-LINK GDB server and more.
     

Get started in 30 seconds

Install on Windows (PowerShell):

irm https://developer.st.com/bundles/install/install.ps1 | iex

Install on macOS or Linux:

curl -fsSL https://developer.st.com/bundles/install/install.sh | bash -

Then, in a project with pinned tool versions — every STM32CubeIDE for VS Code project can pin its tools:

cube bundle install --project        # get exactly the tools this project is pinned to
cube cmake --preset Debug # configure
cube cmake --build --preset Debug # build

 

What changes for you

  • Working on your own: clone, install, build. No setup document, no "which GCC version was it?"
  • Joining a team: productive on day one. The environment comes with the checkout, not from a wiki page someone forgot to update.
  • Leading a team: a tool upgrade becomes a reviewed commit, and you always know which tool versions built a release.
  • Running CI/CD: the build server is not special. Same lock, same tools as the laptop that wrote the code.
     

One lock file, same tools everywhere

Tool versions are recorded in a lock file committed with your project. It holds one entry per operating system and CPU architecture, so the same file gives the right tools on Windows and Linux (x86_64) and on macOS (Intel and Apple silicon). STM32CubeIDE for VS Code, STM32CubeMX2 and the command line all use the same tools underneath.
 

Already using STM32CubeCLT?

STM32CubeCLI gives you the tools you know from STM32CubeCLT, plus per-project version pinning, one registry and one command for all of them. Try it side by side on your next project.
 

Additional resources

Your feedback shapes where STM32CubeCLI goes next. We look forward to reading your ideas and questions on our community forum!


First published on Oct 01, 2026

8 replies

Explorer
Oct 1, 2026 5:22 PM UTC

Ah!!! This is legendary! Thank you for this its great progress.

Associate II
Oct 9, 2026 12:33 PM UTC

If the user has multiple instances of curl on the path the powershell install script fails.
Line #10 stores multiple paths which then get used in line #93. 
E.g. output of “(Get-Command -Name curl -CommandType Application -ErrorAction Stop).Source” on line #10
“C:\Windows\system32\curl.exe
C:\msys64\ucrt64\bin\curl.exe”

Explorer
Oct 10, 2026 4:14 AM UTC

I saw this same issue with my msys installation. Just remove one from path or make the command specifically use one

ST Employee
Oct 15, 2026 7:44 AM UTC

New version of PowerShell script is published to address the issue. 

Associate
Oct 22, 2026 9:26 AM UTC

It would be better to create a fast graphical interface for this command-line tool, instead of developing that terrible CubeIDE or awful VSCode extension.

SKled.1
Senior
Oct 30, 2026 10:05 AM UTC

Tool versions are recorded in a lock file committed with your project

[emphasis mine]


If that “.settings” folder is the same that CubeIDE produces and “feels like” all 3 minutes produces BS changes in some xml files that would produce non-meaningful bogus commits - then no, most certainly it will not be in the repo, but in the .gitignore (via the  folder) ;-)
 

ST Employee
Oct 30, 2026 12:36 PM UTC

Tool versions are recorded in a lock file committed with your project

[emphasis mine]


If that “.settings” folder is the same that CubeIDE produces and “feels like” all 3 minutes produces BS changes in some xml files that would produce non-meaningful bogus commits - then no, most certainly it will not be in the repo, but in the .gitignore (via the  folder) ;-)
 

Hi SKled.1
it is not the same file as CubeIDE uses, the bundle lock file, is actually two new files 

.settings/bundle.store.json
.settings/bundles-lock.store.json

The bundle.store file contains your requested versions.

{
"bundles": [
{
"name": "cmake",
"version": "^4.4.0+st.1"
}
]
}

If you want to keep tools used for this project then this should be added to git.

In this example i initialize the bundle project and add cmake@4.4.0+st.1 to my project.

$ cube bundle init --project cmake

the bundles-lock.store files contains the actually used versions, so to get reproducible builds and select the same versions of all tools on CI or for other developers this should also be added to git.

To use the same same versions of bundles in another checkout of your git repo.

$ cube bundle install --project

Will use the bundle versions specified in the bundles-lock.store file.