Skip to main content
fctu
Associate II
May 20, 2020
Solved

Using STM32CubeProgrammer (v2.2.0) to program SD card of our board (the board is base on STM32MP157C-DK2) but fail and get error message Error: Start operation failed at partition 0x01 Error: TSV flashing service failed

Hi,

Our board is base on STM32MP157C-DK2 and the HW difference are...

1. DK2 CN7 USB Type-C is replaced by micro USB and removed STUSB1600.

2. DK2 CN6 PWR-IN is replaced by DC jack and CC1 is 0.4v to PA4 and CC2 keep 0v to PA5.

And we would like to program SD card (16GB, 8GB) by STM32CubeProgrammer with FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv

The programmer can connect to our board via USB and this tsv is work to program DK2.

Meanwhile the BOOT pin configures as USB mode (000b).

Show the entire log as below:

17:58:45 : STM32CubeProgrammer API v2.2.0

18:01:10 : Read TSV File: D:\AIRD\LiDAR\firmware\release_image\DK2\DK2-Trusted\FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv

18:01:10 : Number of partitions: 9

18:01:50 : USB speed : High Speed (480MBit/s)

18:01:50 : Manuf. ID : STMicroelectronics

18:01:50 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

18:01:50 : SN : 004D00363139511138313636

18:01:50 : FW version : 0x0110

18:01:50 : Device ID : 0x0500

18:01:56 : Start Embedded Flashing service

18:01:56 : Memory Programming ...

18:01:56 : Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32

18:01:56 : File : tf-a-stm32mp157c-dk2-trusted.stm32

18:01:56 : Size : 245364 Bytes

18:01:56 : Partition ID : 0x01

18:01:56 : Download in Progress:

18:01:57 : File download complete

18:01:57 : Time elapsed during download operation: 00:00:00.662

18:01:57 : RUNNING Program ...

18:01:57 : PartID: :0x01

18:01:57 : Error: Start operation failed at partition 0x01

18:01:57 : Error: TSV flashing service failed

18:01:57 : Warning: Connection to device 0x500 is lost

18:01:57 : Disconnected from device.

Please advise the possible reason and hint.

Many Thanks.

FC. Tu

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
May 26, 2020

Hi @fctu​ 

Thanks for clarification. Seems then to be a classical issue, that may have various root cause, and for which we have provided this FAQ article :

https://community.st.com/s/article/FAQ-STM32MP1-STM32CubeProgrammer-USB-reconnect-error-at-STM32MP1-boot-device-flashing

Hope this help,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

4 replies

Olivier GALLIEN
ST Technical Moderator
May 25, 2020

Hi @fctu​ 

Even if your board design is very close to DK2 there is a high risk that boot chain and particularly TF-A does not fit.

Did you check console log while programming ? I guess you will notice a failure in TF-A execution. ( explaining why you can't proceed further in flash operation)

Please consider to recompile TF-A with a Device Tree fitting perfectly your design :

https://wiki.st.com/stm32mpu/wiki/How_to_create_your_board_device_tree

Hope it help,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
fctu
fctuAuthor
Associate II
May 26, 2020

Hi OlivierG,

The programmer can proceed the flash operation since update DTS to TF-A and U-boot.

But the process is stuck on "reconnecting the device ..."

Below is STM32CubeProgrammer log:

=============================================================

19:23:38 : USB speed : High Speed (480MBit/s)

19:23:38 : Manuf. ID : STMicroelectronics

19:23:38 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

19:23:38 : SN : 003600413139511138313636

19:23:38 : FW version : 0x0110

19:23:38 : Device ID : 0x0500

19:23:41 : Start Embedded Flashing service

19:23:41 : Memory Programming ...

19:23:41 : Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32

19:23:41 : File : tf-a-stm32mp157c-dk2-trusted.stm32

19:23:41 : Size : 245364 Bytes

19:23:41 : Partition ID : 0x01

19:23:41 : Download in Progress:

19:23:42 : File download complete

19:23:42 : Time elapsed during download operation: 00:00:00.663

19:23:42 : RUNNING Program ...

19:23:42 : PartID: :0x01

19:23:42 : Start operation done successfully at partition 0x01

19:23:42 : Flashlayout Programming ...

19:23:42 : Running Flashlayout Partition ...

19:23:42 : Flashlayout partition started successfully

19:23:42 : Memory Programming ...

19:23:42 : Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32

19:23:42 : File : u-boot-stm32mp157c-dk2-trusted.stm32

19:23:42 : Size : 801519 Bytes

19:23:42 : Partition ID : 0x03

19:23:42 : Download in Progress:

19:23:43 : File download complete

19:23:43 : Time elapsed during download operation: 00:00:01.571

19:23:43 : RUNNING Program ...

19:23:43 : PartID: :0x03

19:23:43 : reconnecting the device ...

19:24:13 : Error: unable to reconnect the target device: time out expired

19:24:13 : Error: Start operation failed at partition 0x03

19:24:14 : Error: TSV flashing service failed

19:24:14 : Warning: Connection to device 0x500 is lost

19:24:14 : Disconnected from device.

===========================================================

Board side message log as below:

===========================================================

NOTICE: CPU: STM32MP157CAC Rev.?

NOTICE: Model: STMicroelectronics STM32MP157C-DK2 Discovery Board

INFO:  Reset reason (0x15):

INFO:  fc.tu@coretronic.com

INFO:   Power-on Reset (rst_por)

INFO:  Using USB

INFO:   Instance 2

INFO:  Boot used partition fsbl1

NOTICE: BL2: v2.0-r1.5(debug):

NOTICE: BL2: Built : 07:56:09, Nov 5 2019

INFO:  BL2: Doing platform setup

INFO:  PMIC version = 0x21

INFO:  RAM: DDR3-1066/888 bin G 1x4Gb 533MHz v1.45

INFO:  Memory size = 0x20000000 (512 MB)

INFO:  BL2 runs SP_MIN setup

INFO:  BL2: Loading image id 4

INFO:  Loading image id=4 at address 0x2fff0000

INFO:  Image id=4 loaded: 0x2fff0000 - 0x30000000

INFO:  BL2: Loading image id 5

INFO:  GETSTATUS :

INFO:          DFU_STATE_IDLE

INFO:  Receive DFU abort

INFO:  GETSTATUS :

INFO:          DFU_STATE_IDLE

INFO:  UPLOAD :

INFO:          Phase ID : 0

INFO:          address 0x2ffee780

INFO:  GETSTATUS :

INFO:          DFU_STATE_IDLE

INFO:  GETSTATUS :

INFO:          DFU_STATE_IDLE

INFO:  UPLOAD :

INFO:          Phase ID : 0

INFO:          address 0x2ffee780

INFO:  GETSTATUS :

INFO:          DFU_STATE_IDLE

INFO:  Start Download partition 0 to address 0xc0000000 length 0

INFO:  USB : DFU : end of download partition : 0

INFO:  Loading image id=5 at address 0xc0100000

INFO:  GETSTATUS :

INFO:          DFU_STATE_IDLE

INFO:  UPLOAD :

INFO:          Phase ID : 3

INFO:          address 0x2ffee780

INFO:  GETSTATUS :

INFO:          DFU_STATE_IDLE

INFO:  GETSTATUS :

INFO:          DFU_STATE_IDLE

INFO:  UPLOAD :

INFO:          Phase ID : 3

INFO:          address 0x2ffee780

INFO:  GETSTATUS :

INFO:          DFU_STATE_IDLE

INFO:  usb_partition_size: partition size : 0xc39ef

INFO:  Start Download partition 3 to address 0xc0100000 length 801263

INFO:  USB : DFU : end of download partition : 3

WARNING: Skip signature check (header option)

INFO:  GETSTATUS :

INFO:          DFU_STATE_IDLE

INFO:  UPLOAD :

INFO:          Phase ID : 0

INFO:          address 0xffffffff

INFO:  Send detach request

INFO:  GETSTATUS :

INFO:          DFU_STATE_IDLE

INFO:  Receive Detach

INFO:  Image id=5 loaded: 0xc0100000 - 0xc01c39ef

INFO:  read version 0 current version 0

NOTICE: BL2: Booting BL32

INFO:  Entry point address = 0x2fff0000

INFO:  SPSR = 0x1d3

INFO:  PMIC version = 0x21

NOTICE: SP_MIN: v2.0-r1.5(debug):

NOTICE: SP_MIN: Built : 06:47:11, Nov 5 2019

INFO:  ARM GICv2 driver initialized

INFO:  stm32mp HSI (18): Secure only

INFO:  stm32mp HSE (20): Secure only

INFO:  stm32mp PLL2 (27): Secure only

INFO:  stm32mp PLL2_R (30): Secure only

INFO:  SP_MIN: Initializing runtime services

INFO:  SP_MIN: Preparing exit to normal world

U-Boot 2018.11-stm32mp-r3 (May 21 2020 - 19:18:21 +0800)

CPU: STM32MP157CAC Rev.?

Model: STMicroelectronics STM32MP157C-DK2 Discovery Board

Board: stm32mp1 in trusted mode (st,stm32mp157c-dk2)

DRAM: 512 MiB

Clocks:

- MPU : 650 MHz

- MCU : 208.878 MHz

- AXI : 266.500 MHz

- PER : 24 MHz

- DDR : 533 MHz

NAND: 0 MiB

MMC:  STM32 SDMMC2: 0, STM32 SDMMC2: 1

In:  serial

Out:  serial

Err:  serial

invalid MAC address in OTP 00:00:00:00:00:00Net:

Error: ethernet@5800a000 address not set.

eth-1: ethernet@5800a000

Hit any key to stop autoboot: 0

Boot over usb0!

partitions : Writing GPT: success!

done

DFU alt info setting: done

=========================================================

And WINDOWS's device manager cannot recognize this USB device as well.

I'm trying to figure out why the USB connection will be lost when reconnecting.

I appreciate your any feedback.

Many Thanks.

FC

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
May 26, 2020

Hi @fctu​ 

Thanks for clarification. Seems then to be a classical issue, that may have various root cause, and for which we have provided this FAQ article :

https://community.st.com/s/article/FAQ-STM32MP1-STM32CubeProgrammer-USB-reconnect-error-at-STM32MP1-boot-device-flashing

Hope this help,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
fctu
fctuAuthor
Associate II
May 26, 2020

Hi OlivierG,

Thanks for your helping, the problem had been solved.

The root cause was the OTG_VBUS did not wire properly since we removed STUSB1600.

The DFU function is working well now.

Many Thanks,

FC