Skip to main content
sergei.poselenov
Associate
March 2, 2026
Question

Use of STM32CubeMX 6.17.0 with openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11

Hello,

I Installed STM32CubeMX v6.17.0 with STM32MP2 Software Pack 1.3.0.

I see that code generated for CA35 differs from the one generated by the previous version of STM32CubeMX v6.16.1.

 

By the diff below I see that 6.17.0 expects Yocto tree version openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18:

- model = "STMicroelectronics STM32MP257F-DK STM32CubeMX board - openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11";
+ model = "STMicroelectronics STM32MP257F-DK STM32CubeMX board - openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18";

 

These are not the only differences between CubeMX versions, there are more in the .dts/dtsi definitions.

In the Project Manager window I see that the OpenSTLinux Manifest version is set to openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18.

However I'm not planning to switch to Yocto openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18 just now.

Is it possible to use CubeMX v6.17.0 with the older Yocto  tree version openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11?

 

Regards,

Sergei

1 reply

Olivier GALLIEN
ST Technical Moderator
March 2, 2026

Hi @sergei.poselenov ,

CubeMX version is indeed always strongly related to an associate OpenSTLinux release.

DeviceTree generated with 6.17 will likely generate error if compiled with openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11 source and SDK. 

Better to stick on 6.16.1. 

Olivier 

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.