Skip to main content
Associate III
August 26, 2024
Solved

USB and ST-Link can't be plugged in at the same time for the STM32MP257F-EV1 board

Hello, 

I am trying to work on the STM32MP257F-EV1 development board and am running into an interesting issue. Whenever I have both the USB (For booting) and the ST-Link (For power and using minicom) plugged in at the same time booting the image to the board doesn't work, it will boot up to partition 0x03 and then reconnect and start over until I force cancel it. Is there anything I can do in order to allow both of those to be plugged in at the same time?

 

Thanks,

Carson

This topic has been closed for replies.
CarsonBest answer
Associate III
September 18, 2024

Hi Oliver, 

 

I figured out that most of my problems stemmed from using ST link to supply power instead of the Jack. When I changed that the problems seemed to go away. Also switching to a linux machine helped. Thanks!

 

Carson

2 replies

Olivier GALLIEN
ST Technical Moderator
September 2, 2024

Hi @Carson 

Can you please precise in which boot mode you are ? 

Serial boot mode to flash the board or SDCard/eMMC boot mode ? 

Sharing the trace you get on console might help to investigate what's going wrong

Olivier 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
CarsonAuthorBest answer
Associate III
September 18, 2024

Hi Oliver, 

 

I figured out that most of my problems stemmed from using ST link to supply power instead of the Jack. When I changed that the problems seemed to go away. Also switching to a linux machine helped. Thanks!

 

Carson