Skip to main content
jumman_JHINGA
Senior III
November 27, 2025
Question

USART6 causes system reset & SSH failure on STM32MP257F-DK when enabled in DTS (OSTL 6.6.78-stm32mp-r2)

 

Hello ST team,

I am facing a reproducible issue with USART6 on the STM32MP257F-DK board when working with the OpenSTLinux 6.6.78-stm32mp-r2 distribution.

1. Summary of the Problem

When I enable USART6 in the Linux Device Tree and deploy the DTB on the target:

  • SSH access breaks completely after reboot
    (ssh root@192.168.7.1 no longer works)

  • When running a simple A35 UART6 echo application via minicom,
    the entire board resets.

  • The reset is triggered by RIFSC / SERC firewall exceptions.

The very same DTS configuration works perfectly on OpenSTLinux 6.6.48 —
no SSH issue, no kernel panic, and UART6 user application runs fine.

This strongly suggests a firewall / RIF / OP-TEE integration regression between OSTL 6.0.0 and 6.6.78.


2. DTS Snippet That Triggers the Problem

 

 
&usart6 {
 pinctrl-names = "default", "idle", "sleep";
 pinctrl-0 = <&usart6_pins_a>;
 pinctrl-1 = <&usart6_idle_pins_a>;
 pinctrl-2 = <&usart6_sleep_pins_a>;
 status = "okay";

 /* even deleting DMA properties does not avoid the crash */
 /delete-property/dmas;
 /delete-property/dma-names;
};

As soon as this node is active, the issue appears.


3. Crash Log When Running a Simple UART Application

When executing a simple UART send/receive application on ttySTM6,
the board resets with SError and OP-TEE panic:

E/TC:0 stm32_serc_handle_ilac:133 SERC exceptions [63:32]: 0x10
E/TC:0 stm32_serc_handle_ilac:139 SERC exception ID: 36
[ 321.848663] SError Interrupt on CPU1, code 0x00000000bf000002 -- SError
[ 321.848691] Hardware name: STMicroelectronics STM32MP257F-DK Discovery Board (DT)
[ 321.848863] Kernel panic - not syncing: Asynchronous SError Interrupt
...
[ 322.122425] ---[ end Kernel panic - not syncing: Asynchronous SError Interrupt ]---
E/TC:0 Panic 'Watchdog' at stm32_iwdg.c:218 <stm32_iwdg_it_handler>

This suggests:

  • RIF / SERC access violation on USART6 peripheral or DMA/LLI RAM

  • OP-TEE halting system due to firewall violation


4. Observations

  • Issue occurs only in OpenSTLinux 6.6.78-stm32mp-r2.

  • No issue in OSTL 6.0.0 with the same DTS and same application.

  • Removing DMA for USART6 does not prevent OP-TEE SERC panic.

  • USART6 appears in:

    • Kernel DTS

    • OP-TEE RIF protection DTS (stm32mp257f-dk-ca35tdcid-rif.dtsi)

  • Suspected regression:

    • RIFSC default configuration for USART6 changed

    • CID filtering / semaphore / privilege setup may be stricter in 6.6.78

    • OP-TEE RIFPROT macro now requires 8 arguments instead of 5 (breaking older config)


5. Request for Clarification

Could ST confirm whether:

  1. USART6 requires an explicit RIF configuration in OP-TEE in OSTL 6.6.78?

  2. The default RIFPROT configuration for USART6 changed between 6.0.0 and 6.6.78?

  3. There is any known issue with:

    • DMA3 LLI memory region

    • USART6 CID filtering

    • Missing SCID / privilege attributes in the RIF dtsi?

Any guidance on the correct OP-TEE RIF protection entry for USART6 would be appreciated.


6. Setup

  • Board: STM32MP257F-DK

  • OS: OpenSTLinux 6.6.78-stm32mp-r2

  • OP-TEE: 4.0.0-stm32mp-r2 (supplied with OSTL)

  • Boot: SD card

  • Reproduction: 100% consistent


Please advise how USART6 is meant to be configured under OSTL 6.6.x and whether any RIF updates are required in the OP-TEE DT for correct operation.

Thank you.

5 replies

Christophe Guibout
ST Technical Moderator
December 1, 2025

Hello @jumman_JHINGA,

 

Feel free to have a look into this conversation.

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
jumman_JHINGA
Senior III
December 1, 2025

link is not reachable .

Christophe Guibout
ST Technical Moderator
December 1, 2025

My bad : link updated.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
jumman_JHINGA
Senior III
December 4, 2025

I disabled the M33 firmware loading using the following commands:

systemctl stop st-m33firmware-load.service
systemctl disable st-m33firmware-load.service

 

tAfter that, I updated the Device Tree to include the USART6 clock configuration:

&usart6 {
	pinctrl-names = "default", "idle", "sleep";
	pinctrl-0 = <&usart6_pins_a>;
	pinctrl-1 = <&usart6_idle_pins_a>;
	pinctrl-2 = <&usart6_sleep_pins_a>;
	/* uart-has-rtscts; */
	clocks = <&rcc CK_KER_USART6>;
	status = "okay";
};

With these changes, UART6 works correctly and I no longer encounter the SERC-related kernel panic.

However, the SSH connection still drops whenever USART6 is enabled in the DTS.

Following the guidance from this ST post:
https://community.st.com/t5/stm32-mpus-embedded-software-and/stm32mp257-usart-and-serc-exception/m-p/860815#M5358

I removed the _TRACE flag from USBPD_DRP_UCSI, recompiled the firmware, and redeployed the ELF to the target. After re-enabling the M33 firmware, the behavior remains the same: SSH stays down as long as USART6 is enabled in the DTS. Disabling the USART6 node immediately restores SSH functionality.

I would appreciate further guidance on what may still be triggering this conflict between USART6 and the SSH/network subsystem.

 

Lead
January 29, 2026

@jumman_JHINGA @Christophe Guibout 

The clock

clocks = <&rcc CK_KER_USART6>;

Is already defined inside the node. Look at the "stm32mp251.dtsi" file of the linux kernel.

It's werid that you need to include that line in your device tree. This must be a bug I guess...

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer