Skip to main content
Niklas Voi
Associate II
November 4, 2021
Question

STM32Prog CLI and OTP Disply

Hi,

i currently trying to interact via shellscript and stm32cubeprog cli with my stm32mp157 board.

I can run and load tfa and than uboot. But when i want to read otp, my operations get stuck.

What is the correct call for this?

In my Script is use the following :

.../STM32_Programmer_CLI --connect port=usb1 -tm 20000 serial --verbosity 1 -tm 5000 --write ./tfa_und_uboot_slow.tsv --go 0x03 -otp displ

This is my TSV:

#Opt Id Name Type IP Offset Binary

- 0x01 fsbl1-boot Binary none 0x0 ./tf-a-slow-usb.stm32

- 0x03 ssbl-boot Binary none 0x0 ./uboot-slow-usb.stm32

${PROGRAMMER_BINARY} --write ./tfa_und_uboot_slow.tsv --go 0x03 -otp displ

This is the output:

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.8.0          

   -------------------------------------------------------------------

Warning: Timeout is forced to 5000 ms

USB speed  : High Speed (480MBit/s)

Manuf. ID  : STMicroelectronics

Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

SN     : 0046002A3139510B38313636

FW version : 0x0110

Device ID  : 0x0500

Device name : STM32MP1

Device type : MPU

Device CPU : Cortex-A7

Start Embedded Flashing service

Memory Programming ...

Opening and parsing file: tf-a-slow-usb.stm32

 File     : tf-a-slow-usb.stm32

 Size     : 213310 Bytes

 Partition ID : 0x01 

Download in Progress:

[==================================================] 100% 

File download complete

Time elapsed during download operation: 00:00:00.375

RUNNING Program ... 

 PartID:   :0x01 

Error: an error occured while setting virtual partition 0xF1 alternate setting

Error: Start operation failed at partition 0x01

Error: TSV flashing service failed

RUNNING Program ... 

 Address:   : 0x3

Error: Start operation failed

Error: Connection to target must be established before performing any OTP command.

Many thanks for any hints :)

This topic has been closed for replies.

4 replies

PatrickF
ST Employee
November 5, 2021

Hi,

please try:

.../STM32_Programmer_CLI -c port=usb1 -w ./tfa_und_uboot_slow.tsv -otp displ

Works with a similar command line on my STM32MP157F-DK2 board with a simple '2 binaries' TSV file as yours.

#Opt	Id	Name	Type	IP	Offset	Binary
-	0x01	fsbl1-boot	Binary	none	0x0	arm-trusted-firmware/tf-a-stm32mp157f-dk2-usb.stm32
-	0x03	fip-boot	Binary	none	0x0	fip/fip-stm32mp157f-dk2-trusted.bin

Ensure your board is in DFU mode (empty flash or BOOT pins=0b000).

If issues, please check board UART console log.

Are you sure that your TF-A and uBoot are working ?

Regards.

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Niklas Voi
Associate II
November 9, 2021

Hi Patrick,

i tried, but no i get stucked in the TF-A:

Now i get the following Message:

WARNING: VDD unknown

INFO:  Reset reason (0x15):

INFO:   Power-on Reset (rst_por)

INFO:  Using USB

INFO:   Instance 2

INFO:  Boot used partition fsbl1

ERROR:  Boot interface 6 not supported

PANIC at PC : 0x2ffca199

Exception mode=0x00000016 at: 0x2ffca199

Niklas Voi
Associate II
November 10, 2021

Also some tries later i get into uboot ( when i connect on UART4 )

There is following message:

RUNNING Program ... 

 PartID:   :0x03 

Reconnecting the device ...

On the console:

    scanning usb for storage devices... 0 Storage Device(s) found

partitions : done

Phase=END

DFU alt info setting: done

PatrickF
ST Employee
November 22, 2021

Hi,

I think your TF-A and uBoot are not correctly setup regarding your custom HW.

May I suggest to look at following articles:

https://wiki.st.com/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board

https://community.st.com/s/article/FAQ-STM32MP1-Bring-up-procedure

https://community.st.com/s/article/FAQ-STM32MP1-bring-up-troubleshooting-guide

note that if you use CubeProgrammer with UART instead of USB, you should also use a different TF-A binary than for USB (ending with ...uart.stm32 instead of ...usb.stm32).

See https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#Using_STM32Programmer_over_UART

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent