Skip to main content
Associate II
June 9, 2025
Solved

STM32MP257DK SD-Card Writing with STM32CubeProgrammer

I want to use a different SD Card than the one provided with the STM32MP257DK board. I complete writing to the SD Card through STM32CubeProgrammer in boot mode, but STM32CubeProgrammer disappears without the last complete message.
After that, booting does not work even if I do SD boot, and the SD Card is not partitioned.
Are there any separate regulations for the SD Card that should be used with the STM32MP257DK board?

 

INFO: Boot used partition fsbl1
NOTICE: BL2: v2.10-stm32mp2-r1.0(debug):lts-v2.10.5-dirty(7c229848)
NOTICE: BL2: Built : 16:19:31, Jun 28 2024
INFO: EventBuffer0: BuffArea=e03f000 DmaAddr=0e03f000 CoherentMapAddr=0xe03f000
INFO: dwc3_set_dev_speed = HighSpeed
INFO: DFU USB START...
INFO: Event: Link Status Change : ON(0)
INFO: Event: Link Status Change : Early Suspend(5)
INFO: Event: Link Status Change : L2(3)
INFO: Event: Suspend
INFO: USB Suspend mode
INFO: Event: Device Reset
INFO: Event: Device Connection Done
INFO: dwc3_get_dev_speed = HighSpeed
INFO: Event: Link Status Change : ON(0)
ERROR: usb_core_ctl_error : Send an ERROR

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
June 11, 2025

Hi @Kevin_Woo 

did you use a virtual machine or a native Linux PC ?

Could your try at first a basic optee image using CubeProgrammer in command line ?

https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer#How_to_flash_with_STM32CubeProgrammer

commend should be like this one:

./bin/STM32_Programmer_CLI.exe -c port=usb1 -w flashlayout_st-image-weston/optee/FlashLayout_sdcard_stm32mp257f-dk-optee.tsv

 

Regards,

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

5 replies

Kevin_WooAuthor
Associate II
June 9, 2025

I created a partition of the SD Card in advance according to the explanation in https://wiki.st.com/stm32mpu/wiki/How_to_populate_the_SD_card_with_dd_command.

 

After that, I ran stm32cubeprogrammer, but STm32cubeprogrammer disappeared and the program was not completed. core@lge-c:~/share/stm32mpu_dev/Starter-Package/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.12.05/images/stm32mp2/scripts$ ./create_sdcard_from_flashlayout.sh ../flashlayout_st-image-weston/optee/FlashLayout_sdcard_stm32mp257f-dk-ca35tdcid-ostl-m33-examples-optee.tsv

 

 

Kevin_WooAuthor
Associate II
June 9, 2025

sudo dd if=../flashlayout_st-image-weston/optee/../../FlashLayout_sdcard_stm32mp257f-dk-ca35tdcid-ostl-m33-examples-optee.raw of=/dev/sdc bs=8M conv=fdatasync status=progress I wrote FlashLayout_sdcard_stm32mp257f-dk-ca35tdcid-ostl-m33-examples-optee.raw to the SD-Card and created a bootable device.
However, (1) writing does not work properly via STM32CubeProgrammer via USB.
(2) The booting image via the raw file is different from the booting image using the SD-Card provided by DK. (* Example) RAW file: DR Port: USB 2.0, DK-SD: DR Port: USB 3.0)

Kevin_WooAuthor
Associate II
June 9, 2025

Even on the stm32mp157-dk1 board, if you first set up a partition on a new sd card and then execute write using stm32cubeprogrammer, you can see the error message below on the console. Even if you connect 5V/3A to the power port, you can see the same error message. Please also recommend a solution for this part.

 

 


U-Boot 2023.10-stm32mp-r1 (Oct 02 2023 - 14:39:59 +0000)

CPU: STM32MP157DAC Rev.Z
Model: STMicroelectronics STM32MP157D-DK1 Discovery Board
Board: stm32mp1 in trusted mode (st,stm32mp157d-dk1)
Board: MB1272 Var3.0 Rev.C-03
DRAM: no /fwu-mdata node ?
512 MiB
optee optee: OP-TEE: revision 4.0 (2a5b1d12)
I/TC: Reserved shared memory is disabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are disabled
Clocks:
- MPU : 800 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
Core: 379 devices, 40 uclasses, devicetree: board
WDT: Started watchdog with servicing every 1000ms (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 0
Loading Environment from nowhere... OK
In: serial
Out: serial
Err: serial
Previous ADC measurements was not the one expected, retry in 20ms
****************************************************
* WARNING 500mA power supply detected *
* Current too low, use a 3A power supply! *
****************************************************

Net: eth0: ethernet@5800a000
No EFI system partition
No EFI system partition
Failed to persist EFI variables
Hit any key to stop autoboot: 0
Boot over usb0!
DFU alt info setting: done
crq->brequest:0x0

PatrickF
PatrickFBest answer
ST Employee
June 11, 2025

Hi @Kevin_Woo 

did you use a virtual machine or a native Linux PC ?

Could your try at first a basic optee image using CubeProgrammer in command line ?

https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer#How_to_flash_with_STM32CubeProgrammer

commend should be like this one:

./bin/STM32_Programmer_CLI.exe -c port=usb1 -w flashlayout_st-image-weston/optee/FlashLayout_sdcard_stm32mp257f-dk-optee.tsv

 

Regards,

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Kevin_WooAuthor
Associate II
June 11, 2025

Thanks for your reply.
First, I was able to activate the new SD Card using the SD Card access method in Deep Dive.
Afterwards, I verified that the update was possible using STM32CubeProgrammer by selecting the DK-optee.tsv mentioned by PatrickF instead of the tsv file mentioned in the Getting Started page.

I will finish the work in progress and analyze the differences between the various TSV files on the STM32MP257DK board.

Regards