Skip to main content
FKaes.1
Associate III
Nov 23, 2026 5:15 PM UTC
Question

STM32MP157f-dk2 eval board: Problems to connect with STLINK to M4

Hello, 

I wanted to learn something about embedded Linux. So, I bought a stm32mp157f-dk2 eval board. I setup a yotco project, so that I can use remote desktop on it.

I took the original M4 example project from the STM32MP1 workshop. Copy&paste via remote desktop and started it. The orange LED is blinking as expected. As next step, build the project with CubeIDE and wanted to debug it.

But I cannot connect to M4. Any idea ?

The StLink/USB is basicly working, because
 - the serial interface / COM port is working
 - the STLINK is show in windows
 - I was able to make a firmware update of the stlink

BR