Skip to main content
debugging
Lead
Apr 1, 2025 4:22 PM UTC
Solved

STM32MP157 ECO 6.0.0 OP-TEE build fails: libgcc.a not found

OPTEE builds fine on ECO 5.0 (just built it right now with ECO SDK 5.0).

OPTEE build fails on ECO 6.0  (SDK 6.0)

Both on the same machine.

Both using the same Cube-MX generated files and build commands used for both ECO versions.

LD build/core/all_objs.o
arm-ostl-linux-gnueabi-ld.bfd: cannot find libgcc.a: No such file or directory

 

 

 

This topic has been closed for replies.
debugging
debuggingBest answer
Lead
Apr 6, 2025 2:08 PM UTC

I overlooked that the issue is actually mentioned in the OP-TEE wiki for the compiler option.

1 reply

debugging
debuggingAuthorBest answer
Lead
Apr 6, 2025 2:08 PM UTC

I overlooked that the issue is actually mentioned in the OP-TEE wiki for the compiler option.