Skip to main content
This topic has been closed for replies.

2 replies

Imen Ezzine
ST Employee
July 29, 2020

Hi FOrtn.1,

I can say that this is related to the image size and the used protocol.  For example for flashing an image of 1GB it is normal to take a good while. Also via USB protocol would be much faster than via UART.

So I would say this seems normal as long as you obtain a successful flashing.

Please don't hesitate to share more feedbacks in the future.

-Imen

PatrickF
ST Employee
July 29, 2020

Hi,

4 hours sound very long and not normal.

Please check you are not using USB 1.x (12Mbit/s) for whatever reason (e.g. very old USB hub, cable issue, DFU driver issue, etc...).

You could then try using a different SD-Card brand.

Starter kit v2.0.0 image programming on STM32MP157C-DK2 take about 8 minutes on my W10 Laptop using CubeProgrammer v2.5.0. This is about 1.5MB/s average.

Usually similar time or slightly faster when using CubeProgrammer on Linux (or Virtual Machine).

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent