Skip to main content
Aziz BRIGUI
ST Technical Moderator
March 3, 2025
Question

STM32CubeProgrammer v2.19 released

We are pleased to announce that STM32CubeProgrammer 2.19 is available

What is new in 2.19:

  • Support for the STM32WBA6xxx microcontrollers:
    • Internal memory programming
    • Option byte/OTP programming
    • RDP regression with password
    • SFI support
  • Support for MCE Noekeon encryption for STM32H7R3/7S3 and STM32H7R7/7S7 microcontrollers
  • Performance enhancement: support for incremental programming
  • Support for endianness management in automatic serial numbering
  • Added key wrapping using coupling and chaining bridge (CCB), supporting DUA key, for the STM32U3
    series microcontrollers
  • Support for flash programming via J-Link for the STM32WB0 series microcontrollers
  • X-CUBE-RSSe and STM32MPUSSP-UTIL packages install and update from server
  • Support for multiple boards for debug authentication

Main fixed issues in 2.19:

Refer to the STM32 microcontroller wiki at:
https://wiki.st.com/stm32mcu/wiki/STM32CubeProgrammer_errata_2.19.0

Known problems and limitations in 2.19:

Refer to the STM32 microcontroller wiki at:

https://wiki.st.com/stm32mcu/wiki/STM32CubeProgrammer_errata_2.19.0

How to get STM32CubeProgrammer 2.19:

  • Under this link
  • Or update your current installation of STM32CubeProgrammer using: Help > Software update

1 reply

debugging
Lead
April 2, 2025

STCubeProgrammer crashes so often on Ubuntu after flashing an MCU (in my case). Anything that can be done about that ? I use an STV3MOD but also the STLINKV2 and several STMF0,F4's..

 

And BTW always need to click on an "OK" in a box after programming is complete. which is always not in the center of the screen. So mouse movements needed.  Perhaps change it to a light or green checkmark  in the GUI,  yellow when its busy, RED when it failed ? so it's not needed to click that annoying box.

Also when programming is in progress, you can still, by accident, click download,  so it will download again after the first completes, Add an option to only allow one programming job at  a time?