Skip to main content
Visitor II
November 20, 2023
Question

STM32CubeProgrammer using to write to nand fail and get error "Bad size for partition"

Hi,

Using own custom board based on stm32mp151

I'm using STM32CubeProgrammer to program to nand, but I'm getting error

Error: ssbl1 (0x6): Bad size for partition 2 (ssbl1) at 0x200000 = 0xfe00000 <> 0x200000 expected

 

my .tsv file is

#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 tf-a-stm32mp15xc-ya151c-256d-t-serialboot.stm32
- 0x03 ssbl-boot Binary none 0x0 u-boot-stm32mp15xc-ya151c-256d-t-trusted.stm32
P 0x04 fsbl Binary(2) nand0 0x00000000 tf-a-stm32mp15xc-ya151c-256d-t-serialboot.stm32
P 0x06 ssbl1 Binary nand0 0x00200000 u-boot-stm32mp15xc-ya151c-256d-t-trusted.stm32
P 0x07 ssbl2 Binary nand0 0x00400000 u-boot-stm32mp15xc-ya151c-256d-t-trusted.stm32

 

And the mtdparts command on u-boot

STM32MP> mtdparts

---mtdparts_init---
last_ids : nand0=nand0
env_ids : nand0=nand0
last_parts: mtdparts=nand0:2m(fsbl),2m(ssbl1),2m(ssbl2),-(UBI)
env_parts : mtdparts=nand0:2m(fsbl),2m(ssbl1),2m(ssbl2),-(UBI)

last_partition : nand0,0
env_partition : nand0,0

---list_partitions---

device nand0 <nand0>, # parts = 4
#: name size offset mask_flags
0: fsbl 0x00200000 0x00000000 0
1: ssbl1 0x00200000 0x00200000 0
2: ssbl2 0x00200000 0x00400000 0
3: UBI 0x0fa00000 0x00600000 0

--- mtd_part_info: partition number 0 for device nand0 (nand0)

active partition: nand0,0 - (fsbl) 0x00200000 @ 0x00000000

defaults:
mtdids : nand0=nand0
mtdparts: mtdparts=nand0:2m(fsbl),2m(ssbl1),2m(ssbl2),-(UBI)

 

Please advise me about the possible solution.

Thanks in advance.

This topic has been closed for replies.

1 reply

Erwan SZYMANSKI
ST Technical Moderator
November 23, 2023

Hello @timetoeatmaffin ,
Maybe this wiki article could help you : https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#NAND_flash_memory

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.