STM32CubeProgrammer Failed to Flash 128GB MicroSD Card on OSD32MP1-RED board
- 2 replies
- 2492 views
STM32CubeProgrammer v2.10, running on Ubuntu to flash a 64GB MicroSD card on OSD32MP1-RED board is successfull, but failed to flash 128GB MicroSD card on the same board.
Same tsv file and image binaries are used. MicroSD Card is 128GB SanDisk Ultra MicroSD XC1.
STM32CubeProgrammer logs end as follows:
RUNNING Program ...
PartID: :0x03
Reconnecting the device ...
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157C?? Rev.Z,
SN : 001800273239511637383434
DFU protocol: 1.1
Board : --
Device ID : 0x0500
Device name : STM32MP157C?? Rev.Z
Device type : MPU
Device CPU : Cortex-A7
Start operation done successfully at partition 0x03
Error: an error occured while uploading data from the virtual partition 0xF1
Received PhaseID == 0xFF, system is going to reboot
Attached debug logs shows failure is due to the dfu_read function receiving WRONG partition name "@fip/0x06" instead of "@virtual/0xf1".
This partition name is passed into the dfu_read function, as "DFU alt settings list" index, through the USB_REQ_SET_INTERFACE message.
It looks STM32CubeProgrammer is sending worng partition index in USB_REQ_SET_INTERFACE message to dfu driver.
Is there any limit on eMMC/SD card size STM32CubeProgrammer can flash.