Skip to main content
kiichi
Associate III
July 27, 2023
Question

STM32CubeProgrammer cannot connect with STLINK-V3SET.

Hello

I detect (regular) ST-LINK v32 with STM2CubeProgrammer, but it remains not connectrd.

Please tell me what is the problem and how to fix this problem. ?

[LOG]

18:18:10 : STM32CubeProgrammer API v2.14.0 | Windows-32Bits
18:18:13 : UR connection mode is defined with the HWrst reset mode
18:18:13 : ST-LINK SN : 002800205553500E20393256
18:18:13 : ST-LINK FW : V3J12M3B5S1
18:18:13 : Board : STLINK-V3SET
18:18:13 : Voltage : 3.33V
18:18:13 : SWD freq : 8000 KHz
18:18:13 : Connect mode: Normal
18:18:13 : Reset mode : Hardware reset
18:18:13 : Device ID : 0x500
18:18:13 : Revision ID : Rev Z

This topic has been closed for replies.

5 replies

ST Technical Moderator
July 31, 2023

Hello @kiichi ,

Try Connect mode: Under reset.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
AScha.3
Super User
July 31, 2023

from my experience this happens if

a. connection is bad (bad contact or long wires)

b. spikes from mains coming in ; if you supply target not from USB (where stlink is also) your connection is prone to catch inductive or capacitive coupled spikes from mains;

i had exactly this behavior here at my PC . "connection lost" every some minutes or an hour.

then plugged in mains -> target supply at the PCs (filtered) master-slave socket strip and cable routed near usb-cable to target; target has mains filter and mains earth also; now debug can run many hours without any problem.(and still 2,5m away from PC , stlinkV3 -target cable about 20cm long, at full speed 24MHz + 16Mhz SWO)

try this.

If you feel a post has answered your question, please click on " Best Answer ".
Sara BEN HADJ YAHYA
ST Technical Moderator
August 1, 2023

Hello @kiichi,

Thanks for your feedback,

STM32CubeProgrammer does not support SWD/J-TAG with MPUs. However, with STM32CubeIDE, you can connect and debug your MPU.

For MPUs, only USB and UART interfaces are supported in STM32CubeProgrammer.

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
kiichi
kiichiAuthor
Associate III
August 7, 2023

Thank you for the advice.
I will check the connection with STM32CubeIDE. thank you.
Kiichi.

kiichi
kiichiAuthor
Associate III
August 7, 2023

I have a question.
When using STM32CubeProgrammer, it was possible to connect STM32MP157F-EV1 with USB-OTG and write to eMMC of STM32MP157F-EV1.
However, STM32CubeProgrammer could not connect with SWD/J-TAG.
Is it possible to connect with SWD/J-TAG with STM32CubeIDE and write to eMMC?
Kiichi.