Skip to main content
dirk.schoebel
Associate
April 14, 2022
Question

STM32CubeMX crashes when generating code for STM32MP151

I have a complex project which i try to use CubeMX to generate the device trees for A-TF, OP-TEE and Linux, as well as code pieces for the M4.

The crash is not visible in the STM32CubeMX.log file, but is printed in stderr:

2022-04-14 14:55:51,876 [INFO] BlockDiagram:2740 - set Specific Code input for plugin: TAMP
2022-04-14 14:55:51,876 [INFO] BlockDiagram:2740 - set Specific Code input for plugin: ETH
2022-04-14 14:55:51,877 [INFO] CodeGenerator:663 - code generatio: config db path: /home/dirks/STMicroelectronics/STM32CubeMX_Pre//db/
java.lang.NumberFormatException: For input string: "LSI_VALUE"
 at java.base/jdk.internal.math.FloatingDecimal.readJavaFormatString(FloatingDecimal.java:2054)
 at java.base/jdk.internal.math.FloatingDecimal.parseFloat(FloatingDecimal.java:122)
 at java.base/java.lang.Float.parseFloat(Float.java:455)
 at com.st.microxplorer.codegenerator.McuDataModel.getIpRCCSourceInfo(McuDataModel.java:939)
 at com.st.microxplorer.codegenerator.McuDataModel.initMcuData(McuDataModel.java:221)
 at com.st.microxplorer.codegenerator.McuDataModel.<init>(McuDataModel.java:162)
 at com.st.microxplorer.codegenerator.CodeGenerator.generateCode(CodeGenerator.java:1220)
 at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.generateCode(ProjectBuilder.java:2369)
 at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createCode(ProjectBuilder.java:1961)
 at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:630)
 at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:54)

Doing the whole pin configuration for more than 100 pins is very time consuming. We are in the process of having a second project with the STM32MP1 (XXXXXXX removed by moderator), so the graphical tool would be extremely helpful.

I tried to generate the code with CubeMX 6.5.0, and also with the XXXXX (removed by moderator), both crash with the same error.

Regards,

Dirk.

This topic has been closed for replies.

4 replies

dirk.schoebel
Associate
April 14, 2022

The problem appears with the STM32MP151 project, independent of the second one.

johnnyc
Associate II
June 13, 2022

We're having exactly the same problem with a STM32MP157 project, stack trace is the following:

java.lang.NumberFormatException: For input string: "LSI_VALUE"
at java.base/jdk.internal.math.FloatingDecimal.readJavaFormatString(FloatingDecimal.java:2054)
at java.base/jdk.internal.math.FloatingDecimal.parseFloat(FloatingDecimal.java:122)
at java.base/java.lang.Float.parseFloat(Float.java:455)
at com.st.microxplorer.codegenerator.McuDataModel.getIpRCCSourceInfo(McuDataModel.java:939)
at com.st.microxplorer.codegenerator.McuDataModel.initMcuData(McuDataModel.java:221)
at com.st.microxplorer.codegenerator.McuDataModel.<init>(McuDataModel.java:162)
at com.st.microxplorer.codegenerator.CodeGenerator.generateCode(CodeGenerator.java:1254)
at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.generateCode(ProjectBuilder.java:2665)
at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createCode(ProjectBuilder.java:2094)
at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:752)
at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:54)

Can anyone from ST help out?

johnnyc
Associate II
June 17, 2022

@Community member​ Can you please have a look, this is urgent for one of our customers.

Sara BEN HADJ YAHYA
ST Technical Moderator
June 21, 2022

Hello @dirk.schoebel​ , @johnnyc​ 

Could you please share a detailed scenario to help me reproduce the issue ?

Thanks,

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.