Skip to main content
ST Technical Moderator
March 2, 2026
Question

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available.

What is new in 6.17.0:

  • Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 series
  • Added support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, STM32H5F5J-DK, and NUCLEO-U3C5ZI-Q
  • Added the Start From Board feature for NUCLEO-U3C5ZI-Q, NUCLEO-H5E5ZJ, and NUCLEO-WBA25CE1
  • Added support for new features:
    • PLAY on STM32H5 devices with 4 Megabytes of flash memory
    • HSP on STM32U3 devices with 2 Megabytes of flash memory 
    • STM32CubeMX Notification Service: allows users to subscribe to notifications, updates, or premium content when downloading or installing STM32 software. The subscription to this service is entirely optional and is not mandatory for downloading or installing the software.​
  • Enhanced the memory management tool for the STM32N6 series
  • Implemented the use of the CMake build generator with STM32MP2 projects
  • Enhanced the build process using CMake
  • Upgraded Jxbrowser version to 8.15.0
  • Added support for Cortex-A35 coprocessor management through the Cortex-M33 nonsecure project
  • Upgraded OpenSTLinux version to OSTL 6.2.0

Main fixed issues in 6.17.0:

Refer to the STM32 microcontroller wiki at:

https://wiki.st.com/stm32mcu/wiki/STM32CubeMX_errata_6.17.x

Known problems and limitations in 6.17.0:

Refer to the STM32 microcontroller wiki at:

https://wiki.st.com/stm32mcu/wiki/STM32CubeMX_errata_6.17.x

How to get STM32CubeMX 6.17.0:

  • Under this link
  • Or update your current installation of STM32CubeMX using: Help > Check for Updates
This topic has been closed for replies.