Skip to main content
Semer CHERNI
ST Employee
July 7, 2025
Question

STM32CubeMX 6.15.0 released

We are pleased to announce that the version 6.15.0 of STM32CubeMX is available.

What is new in 6.15.0:

  • Enhanced microprocessor support: Added the STM32MP21-A35-TD, STM32MP21-M33-TD, STM32MP25-M33-TD, and STM32MP23-M33-TD trusted domains for the STM32MP2 MPUs and their Arm® Cortex®-A35 and Cortex®-M33 processors.
  • Integrated the STARM-Clang toolchain:
    • The STMicroelectronics LLVM-based toolchain for Arm®, STARM-Clang, leverages Clang's modular architecture for faster compilation and enhanced support for modern language standards, expanding the build capabilities.
  • Build process enhancements:
    • Use of CMake for more efficient project compilation.
    • Removal of the -Wpedantic and -Wextra options from CMake GCC toolchain template to match the build results produced by STM32CubeIDE.
  • Updated the RIF feature implementation:
    • Integrated the RIF feature for STM32MP2 microprocessors with the STM32MP21-A35-TD, STM32MP21-M33-TD, STM32MP25-M33-TD, and STM32MP23-M33-TD trusted domains.
  • Updated software download management:
    • Added pause and resume functionalities to the software package download feature.
  • Updated the IAR Embedded Workbench® for Arm® toolchain (EWARM) support:
    • Added the support for STM32MP13xx microprocessors.
  • Updated the pin-to-pin compatibility:
    • Implemented the pinout compatibility for STM32MP2 microprocessors.
  • Added the wM-Bus middleware:
    • Implemented the wM-Bus PHY middleware for STM32WL33xx microcontrollers.
  • Updated the memory management tool (MMT):
    • Implemented memory management for the STM32U3.
  • Upgrade Azure RTOS [USBX ,LevelX ,FileX ,ThreadX]  6.2.0 to 6.4.0 for STM32WBA6​.
  • Upgraded the JxBrowser version to V8.5.0.

Main fixed issues in 6.15.0:

Refer to the STM32 microcontroller wiki at:
https://wiki.st.com/stm32mcu/wiki/STM32CubeMX_errata_6.15.x

Known problems and limitations in 6.15.0:

Refer to the STM32 microcontroller wiki at:

https://wiki.st.com/stm32mcu/wiki/STM32CubeMX_errata_6.15.x

How to get STM32CubeMX 6.15.0:

  • Under this link
  • Or update your current installation of STM32CubeMX using: Help > Check for Updates

1 reply

Associate
November 8, 2025

很好奇,cubemx安装的库中为什么没有cubemx工程示例?