Skip to main content
Semer CHERNI
ST Employee
November 27, 2024
Question

STM32CubeMX 6.13.0 released

We are pleased to announce to you that the release 6.13.0 of STM32CubeMX is available.

What is new in 6.13.0:

  • Added support for the following series, microcontrollers and microprocessors: STM32N6, STM32U3, STM32WL3x, STM32G411xx and STM32C0
  • Added the support for the following Nucleo boards: NUCLEO-N657X0-Q, NUCLEO-C051C8, NUCLEO-C092RC, NUCLEO-U385RG-Q, NUCLEO-WL33CC1 and NUCLEO-WL33CC2
  • Added the support for a new Discovery kits and a new expansion boards: STM32N6570-DK and B-WBA5M-WPAN
  • Extended the implementation of the CMake and Makefile build generators taking into account the memory management tool (MMT) features:
    • Single-core microcontrollers without Arm® TrustZone®(a), excluding STM32H7Rx/7Sx, or with disabled TrustZone®
    • Dual-core microcontrollers without TrustZone® (such as in the STM32H7 series)
  • Add the support of the memory management tool on STM32H7 dual-core and STM32WBA5Mxx microcontrollers
  • Added the compare projects feature to make user able to differentiate between two STM32CubeMX project files across different microcontrollers and microprocessors.
  • Implemented the loading of the firmware or applications code from the external memory (EXTMEMLOADER) using the OpenBootloader interface for STM32H7Rx/7Sx.

Main fixed issues in 6.13.0:

Refer to the STM32 microcontroller wiki at:
https://wiki.st.com/stm32mcu/wiki/Category:STM32CubeMX_errata

Known problems and limitations:

Refer to the STM32 microcontroller wiki at:

https://wiki.st.com/stm32mcu/wiki/STM32CubeMX_errata_6.13.x

How to get STM32CubeMX 6.13.0:

  • Under this link
  • Or update your current installation of STM32CubeMX using: Help > Check for updates
This topic has been closed for replies.