Skip to main content
Semer CHERNI
ST Employee
July 1, 2024
Question

STM32CubeMX 6.12.0 released

We are pleased to announce you that the official release of STM32CubeMX V6.12.0 is available.

  • What is new in STM32CubeMX V6.12.0?
    • New MCUs/MPUs series : STM32WB0 ,STM32MP25XX and STM32C071XX
    • Add support new CPNs STM32G4: Add support STM32G4 'Z’ and STM32G414
    • New Boards are supported: NUCLEO-C071RB , NUCLEO-WB09KE ,NUCLEO-WB07CC ,NUCLEO-WB05KZ ,STM32MP257F-DK , STM32MP257F-EV1
    • Remove STM32MP15 obsolete boards from CubeMX board selector  (  STM32MP157A-DK1 , STM32MP157A-EV1, STM32MP157C-DK2,   STM32MP157C-EV1)
    • New Boards are supported by the Start from Board feature: Nucleo-WB09xx Nucleo-WB07xx ,Nucleo-WB05xx ,Nucleo-C0 , NUCLEO-G431RB ,NUCLEO-G474RE ,NUCLEO-G491RE ,NUCLEO-H503RB ,NUCLEO-U545RE ,NUCLEO-WB15CC ,NUCLEO-WB55RG ,P-NUCLEO-WB55 ,P-NUCLEO-WB55 ,NUCLEO-WL55JC1 ,NUCLEO-WL55JC2 ,NUCLEO-WBA52CG ,NUCLEO-WBA55CG
    • Add CMake support for multicontext projects (Multi-Context ,Trust zone , Multi-core)
    • Add the support of the memory management tool for STM32WB0X and H7SC microcontrollers
    • Updated STM32CubeMX management of option bytes: STM32CubeMX preserves option bytes when regenerating a project  (H7RS ,H5, U0, WBA)
    • Add support feature (Resource Isolation Framework )RIF  / RIF Aware Ips for STM32MP25
    • LPBAM : Add missing ADF1 configuration in the LPBAM function Toolbox 
    • Add support Makefile support for WB09/07/05 and H7RS
  • Main fixed issues:
    • 164664: An issue with GUI display in STM32CubeMX.
    • 166529: TRACESWO is linked to only to Arm® Cortex®-M7 for the dual-core microcontrollers in the STM32H7 series excluding the STM32H7Rx/7Sx microcontrollers.
    • 177884: Unable to uncheck the option "save power of non-active UCPD - deactive Dead Battery pull-up" for the STM32G0 series.
    • 178050: MMC interface mode is greyed out when SDMMC1 is set to"MMC 4 bit wide bus" for the STM32H5 series.
    • 178907/179287: Incomplete generated code related to the MX_ADC3_Init() function for the STM32H7 series
    • 179275: Missing init generated code related to the MX_ADC4_Init() function for the STM32U5 series
    • 179295: Wrong generated code related to the MX_ADC1_Init() function for the STM32L4 series
    • 180281: Issue with Missing 'handle_GPDMA1' in Standard Request Mode for GPDMA Configuration for the STM32U5 series
    • 180548/181495: Oversampling ratio error for ADC3 in STM32CubeMX generated code for the SSTM32H7 series but the STM32H7Rx/7Sx microcontrollers
    • 180967: Build errors in ThreadX project with exclusive selection of LL drivers for the STM32 MCUs
    • 181386: Issue with DAC to ADC internal connection in STM32CubeMX for all the STM32H7 series but the STM32H7Rx/7Sx microcontrollers.
    • 181812: Compilation error related to the custom_stm.c file for the STM32WB series
  • Known issues fixed and problems and limitations:
    • Please refer to the wiki under this link and the release note RN0094.
This topic has been closed for replies.