Skip to main content
Sindel
Associate
May 6, 2021
Question

STM32CubeIDE for OSX for MP1

Is it possible to use the CubeIDE on OSX for debugging firmware for STM32MP1?

The interface is lacking some features and the debugging configuration is completely different.

Also I can't manage to make it work.

Here is what shows up when I launch Debug Configurations:

0693W00000ANb7ZQAT.png

This topic has been closed for replies.

3 replies

Cartu38 OpenDev
Graduate II
May 6, 2021

As far as I'm aware STM32MP1 is not MacOS supported if debug.

Quite old post ... is it still valid ? See https://community.st.com/s/question/0D50X0000BxxoQSSQY/the-stm32cubeide-v110-hasnt-load-image-option-on-macos

Sindel
SindelAuthor
Associate
May 6, 2021

Thanks, I searched for OSX but it did not produce any result. Too bad that there is no support.

Cartu38 OpenDev
Graduate II
May 6, 2021

Compare a Linux install vs. MacOS one ... some debug components are lacking