Skip to main content
Semer CHERNI
ST Employee
July 7, 2025
Question

STM32CubeIDE 1.19.0 released

We are pleased to announce that the release 1.19.0 of STM32CubeIDE is available.

What is new in 1.19.0:

  • Microcontroller, microprocessor, and board lists aligned with STM32CubeMX v6.15.0:
    • Added the support for STM32MP21xx microprocessors to the STM32MP2 series and extended the support for boards based on the STM32MP2 microprocessors
    • Added the support for STM32WL30xx and STM32WL31xx microcontrollers to the STM32WL3x line
  • Added automatic external memory loader prefilling in debug configuration for boards based on the STM32N6 series
  • Added the support for OpenSTLinux 6.1.0 through the update site mechanism
  • Added the support for STM32MP2x-M33-TD projects generated from STM32CubeMX standalone
  • Added the Cortex®-A35 support in the SFRs view
  • Added the capability to install OpenSTLinux through the update site mechanism on empty projects for STM32MP1 and STM32MP2 devices
  • Added the support for TF‑M projects debugging for STM32MP2x-M33-TD
  • Added the new view Flash memories programming allowing the programming of a TSV file for STM32MP1 and STM32MP2 devices in single or dual storage
  • Added the support for new reset strategies when debugging with SEGGER J-Link
  • Added incremental programming as an experimental feature for a defined set of devices:
    • Internal flash memory programming is tested on the following microcontrollers:
      STM32C03xxx, STM32C05xxx, STM32C09xxx, STM32F101/F102/F103, STM32F37xxx,
      STM32F411xC/E, STM32F72xxx, STM32F73xxx, STM32F76xxx, STM32F77xxx, STM32G03xxx,
      STM32G04xxx, STM32G0B0xx/B1xx/C1xx, STM32G491xx, STM32H50xxx, STM32H523/533,
      STM32H562, STM32H563/573, STM32H723/STM32H733, STM32H725/STM32H735, STM32H730
      Value line, STM32H7R3/7S3, STM32H7R7/7S7, STM32L05xxx/L06xxx/L010xx, STM32L4P5/Q5,
      STM32L4x1, /STM32L475xx/STM32L476xx/STM32L486xx, STM32L5, STM32U0, STM32U3,
      STM32U535/545, STM32U575/585, STM32U595/5A5, STM32U599/5A9, STM32WB35xx/5xxx,
      STM32WBA52, STM32WBA54/55, STM32WBA62, STM32WBA63, STM32WBA64/65, and
      STM32WL
    • External flash memory programming is tested on the following boards:
      STM32H735G-DK, STM32H7S78-DK, STM32H573I-DK and STM32U575I-EV

Main fixed issues in 1.19.0:

Refer to the STM32 microcontroller wiki at:

https://wiki.st.com/stm32mcu/wiki/STM32CubeIDE:STM32CubeIDE_errata_1.19.x 

Known problems and limitations in 1.19.0:

Refer to the STM32 microcontroller wiki at:

https://wiki.st.com/stm32mcu/wiki/STM32CubeIDE:STM32CubeIDE_errata_1.19.x 

How to get STM32CubeIDE 1.19.0:

  • Under this link
  • Or update your current installation of STM32CubeIDE using: Help > Check for updates (The intool update does not allow updating the drivers and STLINK server tool. Full installation is required for this to be done).

 

 

This topic has been closed for replies.

2 replies

Associate
July 8, 2025

Hello @Semer CHERNI ,

but code is not generated in STM32CubeIDE 1.19.0

Semer CHERNI
ST Employee
July 9, 2025

Hello @sum1 

I am not able to understand the issue.
What is the scenario, the MCU or Board...

KR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.