Skip to main content
Semer CHERNI
ST Employee
July 1, 2024
Question

STM32CubeIDE 1.16.0 released

STM32CubeIDE 1.16.0 was released today on st.com as well as an in-tool update patch.

  • What is new in 1.16.0?
    • Microcontroller and board lists aligned with STM32CubeMX v6.12.0 : STM32C0 ,STM32WB0 and STM32MP25XX
    • Added CMake support for multicontext projects (Multi-Context ,Trust zone , Multi-core)
    • Added new features for CMake project configuration
    • Basic CMake support now also with Ninja
    • Added the OZ in the optimization level to the build settings
  • Main fixed issues:
    • Refer to the STM32 microcontrollers wiki under this link.
  • Known issues fixed and problems and limitations:
    • Refer to the STM32 microcontrollers wiki under this link.
  • Where do I obtain STM32CubeIDE 1.16.0?
This topic has been closed for replies.

1 reply

Explorer II
November 7, 2024

I've been try 1.16.0 and 1.16.1 with Nucleo-L552ZEQ, but unluckily i can not make it working for debugging. seems debugging not download to flash. But it didn't happen when using cube 1.14.1.

Any idea? thanks