Skip to main content
Semer CHERNI
ST Employee
April 25, 2024
Question

STM32CubeIDE 1.15.1 released

STM32CubeIDE 1.15.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.11.1 that is available for download.

Main issues fixed in this patch:

  • Ticket 177978 : Fixed an issue with ST-LINK firmware upgrade concerning the boards with DFU v2 or older in the version 3.14.5 of ST-LINK GDB server.
  • Ticket 178127 : Fixed an issue with the build settings: The build settings do not save the latest linker modified by the user and select the default linker instead.

Check the errata under this link for more details.

Where do I obtain STM32CubeIDE 1.15.1?

This topic has been closed for replies.

3 replies

Uwe Bonnes
Chief
April 25, 2024

The download page still only offers 1.15.0.

Intector
Senior
April 25, 2024

Hey Uwe,

It'll probably take more than 56 minutes...

 

"Always be yourself. Unless you can be a pirate. Then always be a pirate.”

AScha.3
Super User
April 25, 2024

...seems so.

AScha3_0-1714044305729.png

 

If you feel a post has answered your question, please click on " Best Answer ".