Skip to main content
Visitor II
April 15, 2025
Question

STEVAL-STLKT01V1 Firmware using Blue-ST-Protocol Python

Hello,

I was writing an application interacting with the default firmware on the STEVAL-STLKT01V1 in python using the Blue-ST-SDK and it was working fine (https://github.com/STMicroelectronics/BlueSTSDK_Python/tree/master).  

  My teammate then flashed the FP-SNS-ALLMEMS1 firmware on the tile and now the script I wrote using the Blue-ST-SDK-Python cannot discover it (the example_1.py now simply times out) even though the device MAC address can be found with bluepy.  It gives this error when trying to add the node by the MAC address:

AM1V420: "Manufacturer specific data" must be of length "7" or "13", not "15".

  The board is discoverable and usable by the ST BLE Sensor app.  Maybe the FP-SNS-ALLMEMS1 is only compatible with IOS/Android versions of the SDK?

    Which firmware is compatible with the Blue-St-Protocol-Python?  And which firmware is default flashed onto the Sensortile?  I simply need to read accelerometer and gyroscope data.

Best, Evan

This topic has been closed for replies.