Skip to main content
Associate II
September 3, 2025
Question

ST32MP257F-DK ADC init problem

Hi,

I'm trying to get ADC working on ST32MP257F-DK board. There is no example in ST's sw-package and the example for ST32MP257F-EV1 board fails in HAL_ADC_Init -function giving error messages:

stm32_serc_handle_ilac:134 SERC exceptions [63:32]: 0x8000000
stm32_serc_handle_ilac:140 SERC exception ID: 59

Can somebody help, what is the difference between these boards with ADC? 

(And why there is no ADC example for ST32MP257F-DK?)

    

 

This topic has been closed for replies.

7 replies

Erwan SZYMANSKI
ST Technical Moderator
September 3, 2025

Hello @nh7 ,
Could you please tell me which is the Flash image that you flashed to boot the board ? Did you use a prepared Flash image or did you make your own one ? Did you do any CubeMX configuration yourself for your device trees ? 

The error that you see is a RIF error telling you that you (M33 cortex) is not allowed to use ADC3, which is strange because M33 has access to ADC3 in all our default configuration.

Are you on OpenSTLinux v 6.1 ? 

In your Linux console, can you make a "cat /sys/kernel/debug/stm32_firewall/rifsc" and gives the output ?

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
nh7Author
Associate II
September 16, 2025

Hello,

I made my own image. I have some own configurations in device tree. They are mainly for spi6, should not affect ADC?

I'm using openstlinux-6.1-yocto-mickledore.

Output of "cat /sys/kernel/debug/stm32_firewall/rifsc" is in attached file.

Pwxn
ST Employee
September 17, 2025

Hello,

 

On the file you share we can see:

| Peripheral name || Firewall ID || N/SECURE || N/PRIVILEGED || CID filtering || Semaphore mode || SCID || SEMWL |

| ADC12 || 58 || NSEC || NPRIV || disabled || disabled || 0 || 0x0 |

| ADC3 || 59 || NSEC || NPRIV || disabled || disabled || 0 || 0x0 |

 

If you want to use the ADC with the M33 you need to set the Compartment IDentifier (CID) to 2. You need to reviews your configuration. If you use CubeMX you can quickly see which CID is set for your peripherals as you configure their pinout.  

Pwxn_1-1758089661462.png

 

Finally, you can refer to the RM0457 9.4.6 RIFSC control of peripherals (RISUP) for more details.

I hope this will help you.

 

Regards,

nh7Author
Associate II
September 17, 2025

Hello,

CubeMX looks the same here. Can you tell me which file to edit to get this CID configured?

Pwxn
ST Employee
September 19, 2025

Hello,

 

In the device tree of OPTEE you will find the <machine>-<project>-rif.dtsi

&rifsc {
	st,protreg = <
		RIFPROT(STM32MP25_RIFSC_ADC12_ID, RIF_UNUSED, RIF_UNLOCK, RIF_NSEC, RIF_PRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN)
		RIFPROT(STM32MP25_RIFSC_ADC3_ID, RIF_UNUSED, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIF_CID2, RIF_SEM_DIS, RIF_CFEN)

 

You can modify it manually.

 

Regards, 

GatienC
ST Employee
September 19, 2025

Hi,

I think there is a confusion between IAC and SERC events here.

SERC events occur when there is an access to a peripheral whose clock is disabled or is under reset. This is not related to RIF firewall configuration.

On the other hand, the clock access configuration depends on the ADC RIF configuration. Therefore, if you want to enable the clock, then the ADC must be accessible by the context trying to enable it.

To conclude: please check the clock state of the ADC: (RCC_ADC12CFGR) or (RCC_ADC3CFGR) registers

Best regards,

Gatien

GatienC
ST Employee
September 19, 2025