Skip to main content
Visitor II
February 12, 2026
Question

Secure boot on STM32mp157f

Hi,
I am trying to enable secure boot in STM32mp157f-ev1 board. I am using the Developer Package source code provided by ST. I am using this command to generate the tf-a.stm32:
make E=0 -f ../Makefile.sdk.stm32mp1 TF_A_DEVICETREE=stm32mp157f-ev1 TF_A_CONFIG="optee-sdcard optee-programmer-usb" TRUSTED_BOARD_BOOT=1 GENERATE_COT=1 ROT_KEY=<path>/privatekey.pem ROT_KEY_PWD=<password> KEY_ALG=ecdsa MBEDTLS_DIR=<path>/mbedtls-3.4.1 DYN_DISABLE_AUTH=0 DEPLOYDIR=$FIP_DEPLOYDIR_ROOT/arm-trusted-firmware stm32

But I am getting an error:
LD SOURCES-stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11/sources/ostl-linux/tf-a-stm32mp-v2.10.13-stm32mp-r2-r0/tf-a-stm32mp-v2.10.13-stm32mp-r2/../build/optee-sdcard-stm32mp157f-ev1/bl2/bl2.elf
arm-ostl-linux-gnueabi-ld.bfd: SOURCES-stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11/sources/ostl-linux/tf-a-stm32mp-v2.10.13-stm32mp-r2-r0/tf-a-stm32mp-v2.10.13-stm32mp-r2/../build/optee-sdcard-stm32mp157f-ev1/bl2/bl2.elf section `.xlat_table' will not fit in region `RAM'
arm-ostl-linux-gnueabi-ld.bfd: BL2 image has exceeded its limit.
arm-ostl-linux-gnueabi-ld.bfd: region `RAM' overflowed by 4096 bytes
make[1]: *** [Makefile:1539:SOURCES-stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11/sources/ostl-linux/tf-a-stm32mp-v2.10.13-stm32mp-r2-r0/tf-a-stm32mp-v2.10.13-stm32mp-r2/../build/optee-sdcard-stm32mp157f-ev1/bl2/bl2.elf] Error 1
make[1]: Leaving directory 'SOURCES-stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11/sources/ostl-linux/tf-a-stm32mp-v2.10.13-stm32mp-r2-r0/tf-a-stm32mp-v2.10.13-stm32mp-r2'