Skip to main content
Sindhu Vadde
Associate III
October 8, 2021
Question

Regarding DTS file in Stm32mp157A u boot

Hi,

We are using stm32mp157a-dk1 target.I have an issue i.e,when i use uboot source code dts file in u boot source code its works fine.when i replace original dts with stm32 cubemx generated dts it didn't works.Can i use cube mx generated dts in place of original dts in u boot.

Thanks in advance

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
October 8, 2021

Hi @Sindhu Vadde​ ,

Can you clarify which version of OpenSTLinux you are using and the version of CubeMX ?

Then, in CubeMX did you create a board DK1 project or a sample project ?

When you mean "it didn't work" can you please clarify ? Can you share some logs ?

Thanks

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Sindhu Vadde
Associate III
October 9, 2021

Hi,

Thanks for the reply,

we are using 5.10 dunfell-mp1-21-03-31 open ST Linux and 6.2.0 cube mx version.

we have created project for DK1 not sample project.

when i use cube mx generated dts i didn't get any log.