Skip to main content
Associate II
April 23, 2026
Question

Project compilation error after migration to CubeMX 6.17.0

Hi,


i tried to migrate my project to CubeMx v6.17.0 coming from v6.16.0
As a result, the firmware package was also updated to FW_MP1 V1.7.0

I am using CubeIDE 2.0.0

After migration the compilation fails with following error in auto-generated FreeRTOSConfig.h

Description Resource Path Location Type each undeclared identifier is reported only once for each function it appears in FreeRTOSConfig.h /PROJECT_CM4/Inc line 71 C/C++ Problem
/* USER CODE BEGIN Header */
/*
 * FreeRTOS Kernel V10.6.2
 * Portion Copyright (C) 2017 Amazon.com, Inc. or its affiliates. All Rights Reserved.
 * Portion Copyright (C) 2019 StMicroelectronics, Inc. All Rights Reserved.
 *
 * Permission is hereby granted, free of charge, to any person obtaining a copy of
 * this software and associated documentation files (the "Software"), to deal in
 * the Software without restriction, including without limitation the rights to
 * use, copy, modify, merge, publish, distribute, sublicense, and/or sell copies of
 * the Software, and to permit persons to whom the Software is furnished to do so,
 * subject to the following conditions:
 *
 * The above copyright notice and this permission notice shall be included in all
 * copies or substantial portions of the Software.
 *
 * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
 * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS
 * FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE AUTHORS OR
 * COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER
 * IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN
 * CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE SOFTWARE .
 *
 * http://www.FreeRTOS.org
 * http://aws.amazon.com/freertos
 *
 * 1 tab == 4 spaces!
 */
/* USER CODE END Header */
#ifndef FREERTOS_CONFIG_H
#define FREERTOS_CONFIG_H

/*-----------------------------------------------------------
 * Application specific definitions.
 *
 * These definitions should be adjusted for your particular hardware and
 * application requirements.
 *
 * These parameters and more are described within the 'configuration' section of the
 * FreeRTOS API documentation available on the FreeRTOS.org web site.
 *
 * See http://www.freertos.org/a00110.html
 *----------------------------------------------------------*/

/* USER CODE BEGIN Includes */
/* Section where include file can be added */
/* USER CODE END Includes */

/* Ensure definitions are only used by the compiler, and not by the assembler. */
#if defined(__ICCARM__) || defined(__CC_ARM) || defined(__GNUC__)
#include <stdint.h>
extern uint32_t SystemCoreClock;
/* USER CODE BEGIN 0 */
extern void configureTimerForRunTimeStats(void);
extern unsigned long getRunTimeCounterValue(void);
/* USER CODE END 0 */
#endif
#ifndef CMSIS_device_header
#define CMSIS_device_header "stm32mp1xx.h"
#endif /* CMSIS_device_header */

#define configENABLE_FPU 0
#define configENABLE_MPU 0

#define configUSE_PREEMPTION 1
#define configSUPPORT_STATIC_ALLOCATION 1
#define configSUPPORT_DYNAMIC_ALLOCATION 1
#define configUSE_IDLE_HOOK 0
#define configUSE_TICK_HOOK 0
#define configCPU_CLOCK_HZ ( SystemCoreClock )
#define configTICK_RATE_HZ ((TickType_t)1000)
#define configMAX_PRIORITIES ( 56 )

 

As expected, once I removed cast (TickType_t) for the sake of simplicity, all the problems were solved.
Does anyone have any ideas or suggestions, or do I need to start the project from scratch?

Thanks

 

2 replies

Ghofrane GSOURI
ST Technical Moderator
May 4, 2026

Hello @Jagr 

Could you please provide your IOC?

I will be waiting for your feedback.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JagrAuthor
Associate II
May 5, 2026

Hi,

i will provide the .ioc later.
first i have new insight which might be helpful.
In my old project i had a preprocessor definition 

METAL_FREERTOS

If i remove this from project settings it was possible to compile.