Skip to main content
Associate II
December 8, 2025
Question

Problem configuring kernel for stm32mp157f-dk2 using make menuconfig

Hello,
I'm trying to modify STM32MP157x-DK2 kernel so that it would use ST ethernet drivers (dwmac-stm32.ko, stmmac.ko et al.) as modules (like on stm32mp257f board we have) and not be included into the kernel uImage. I'm using latest v.25.08.27 package and instructions for building and modifying  kernel, and uImage and its default modules are built fine. But when I try to use make menuconfig  to modify build configuration, I receive the following errors:
make menuconfig
GEN Makefile
HOSTLD scripts/kconfig/mconf
/home/###/workspace/DeveloperPackage/SDK_MP1/sysroots/x86_64-ostl_sdk-linux/usr/lib/gcc/x86_64-ostl_sdk-linux/13.3.0/../../../../x86_64-ostl_sdk-linux/bin/ld: scripts/kconfig/mconf.o: in function `show_help':
mconf.c:(.text+0x87a): undefined reference to `stdscr'
/home/###/workspace/DeveloperPackage/SDK_MP1/sysroots/x86_64-ostl_sdk-linux/usr/lib/gcc/x86_64-ostl_sdk-linux/13.3.0/../../../../x86_64-ostl_sdk-linux/bin/ld: scripts/kconfig/lxdialog/checklist.o: in function `print_arrows':
checklist.c:(.text+0x2c): undefined reference to `wmove'
.................
I check and all recommended libraries and packages are installed. Previously when I modified kernel configuration for STM32MP2-157F board, I didn't have such problem. 
Please advise how this issue could be resolved.
Thank you.