Skip to main content
Associate III
August 13, 2024
Solved

Populating the EMMC seems like an infinite download loop

Hello, 

 

I am trying to populate the EMMC on the STM32MP257F-EV1 development board using a USB connection and I am running into a strange issue. I am trying to download the file from this wiki: Populate the target and boot the image - stm32mpu and specifically trying to download "FlashLayout_emmc_stm32mp257f-ev1-ca35tdcid-ostl-m33-examples-optee.tsv". When I do this everything seems fine at first. But it looks like the download may be in an infinite loop. Here is what the Log said from when I started the download to when I stopped it: 

09:58:50 : Number of partitions: 14
09:58:56 : Start Embedded Flashing service
09:58:56 : Memory Programming ...
09:58:56 : Opening and parsing file: tf-a-stm32mp257f-ev1-ca35tdcid-ostl-usb.stm32
09:58:56 : File : tf-a-stm32mp257f-ev1-ca35tdcid-ostl-usb.stm32
09:58:56 : Size : 198.86 KB
09:58:56 : Partition ID : 0x01
09:58:56 : Download in Progress:
09:59:04 : File download complete
09:59:04 : Time elapsed during download operation: 00:00:07.629
09:59:04 : RUNNING Program ...
09:59:04 : PartID: :0x01
09:59:05 : Reconnecting the device ...
09:59:05 : USB speed : High Speed (480MBit/s)
09:59:05 : Manuf. ID : STMicroelectronics
09:59:05 : Product ID : DFU @Device ID /0x505, @Revision ID /0x0000, @Name /STM32MP257FAI Rev.B,
09:59:05 : SN : 002300444136500800353653
09:59:05 : DFU protocol: 1.1
09:59:05 : Board : --
09:59:05 : Device ID : 0x0505
09:59:05 : Device name : STM32MP257FAI Rev.B
09:59:05 : Device type :
09:59:05 : Device CPU :
09:59:05 : Start operation done successfully at partition 0x01
09:59:05 : Memory Programming ...
09:59:05 : Opening and parsing file: fip-stm32mp257f-ev1-ca35tdcid-ostl-ddr-optee-emmc.bin
09:59:05 : File : fip-stm32mp257f-ev1-ca35tdcid-ostl-ddr-optee-emmc.bin
09:59:05 : Size : 29.38 KB
09:59:05 : Partition ID : 0x02
09:59:05 : Download in Progress:
09:59:06 : File download complete
09:59:06 : Time elapsed during download operation: 00:00:00.920
09:59:06 : RUNNING Program ...
09:59:06 : PartID: :0x02
09:59:06 : Reconnecting the device ...
09:59:06 : USB speed : High Speed (480MBit/s)
09:59:06 : Manuf. ID : STMicroelectronics
09:59:06 : Product ID : DFU @Device ID /0x505, @Revision ID /0x0000, @Name /STM32MP257FAI Rev.B,
09:59:06 : SN : 002300444136500800353653
09:59:06 : DFU protocol: 1.1
09:59:06 : Board : --
09:59:06 : Device ID : 0x0505
09:59:06 : Device name : STM32MP257FAI Rev.B
09:59:06 : Device type :
09:59:06 : Device CPU :
09:59:06 : Start operation done successfully at partition 0x02
09:59:06 : Memory Programming ...
09:59:06 : Opening and parsing file: fip-stm32mp257f-ev1-ca35tdcid-ostl-optee-emmc.bin
09:59:06 : File : fip-stm32mp257f-ev1-ca35tdcid-ostl-optee-emmc.bin
09:59:06 : Size : 2.65 MB
09:59:06 : Partition ID : 0x03
09:59:06 : Download in Progress:
10:00:30 : File download complete
10:00:30 : Time elapsed during download operation: 00:01:24.215
10:00:30 : RUNNING Program ...
10:00:30 : PartID: :0x03
10:00:31 : Reconnecting the device ...
10:00:33 : USB speed : High Speed (480MBit/s)
10:00:33 : Manuf. ID : STMicroelectronics
10:00:33 : Product ID : DFU in HS Mode @Device ID /0x505, @Revision ID /0x2000
10:00:33 : SN : 002300444136500800353653
10:00:33 : DFU protocol: 1.1
10:00:33 : Board : --
10:00:33 : Device ID : 0x0505
10:00:33 : Device name : STM32MP257FAI Rev.B
10:00:33 : Device type :
10:00:33 : Device CPU :
10:00:33 : Start operation done successfully at partition 0x03
10:00:33 : Memory Programming ...
10:00:33 : Opening and parsing file: tf-a-stm32mp257f-ev1-ca35tdcid-ostl-usb.stm32
10:00:33 : File : tf-a-stm32mp257f-ev1-ca35tdcid-ostl-usb.stm32
10:00:33 : Size : 198.86 KB
10:00:33 : Partition ID : 0x01
10:00:33 : Download in Progress:
10:00:41 : File download complete
10:00:41 : Time elapsed during download operation: 00:00:07.632
10:00:41 : RUNNING Program ...
10:00:41 : PartID: :0x01
10:00:42 : Reconnecting the device ...
10:00:42 : USB speed : High Speed (480MBit/s)
10:00:42 : Manuf. ID : STMicroelectronics
10:00:42 : Product ID : DFU @Device ID /0x505, @Revision ID /0x0000, @Name /STM32MP257FAI Rev.B,
10:00:42 : SN : 002300444136500800353653
10:00:42 : DFU protocol: 1.1
10:00:42 : Board : --
10:00:42 : Device ID : 0x0505
10:00:42 : Device name : STM32MP257FAI Rev.B
10:00:42 : Device type :
10:00:42 : Device CPU :
10:00:42 : Start operation done successfully at partition 0x01
10:00:42 : Memory Programming ...
10:00:42 : Opening and parsing file: fip-stm32mp257f-ev1-ca35tdcid-ostl-ddr-optee-emmc.bin
10:00:42 : File : fip-stm32mp257f-ev1-ca35tdcid-ostl-ddr-optee-emmc.bin
10:00:42 : Size : 29.38 KB
10:00:42 : Partition ID : 0x02
10:00:42 : Download in Progress:
10:00:43 : File download complete
10:00:43 : Time elapsed during download operation: 00:00:00.920
10:00:43 : RUNNING Program ...
10:00:43 : PartID: :0x02
10:00:43 : Reconnecting the device ...
10:00:43 : USB speed : High Speed (480MBit/s)
10:00:43 : Manuf. ID : STMicroelectronics
10:00:43 : Product ID : DFU @Device ID /0x505, @Revision ID /0x0000, @Name /STM32MP257FAI Rev.B,
10:00:43 : SN : 002300444136500800353653
10:00:43 : DFU protocol: 1.1
10:00:43 : Board : --
10:00:43 : Device ID : 0x0505
10:00:43 : Device name : STM32MP257FAI Rev.B
10:00:43 : Device type :
10:00:43 : Device CPU :
10:00:43 : Start operation done successfully at partition 0x02
10:00:43 : Memory Programming ...
10:00:43 : Opening and parsing file: fip-stm32mp257f-ev1-ca35tdcid-ostl-optee-emmc.bin
10:00:43 : File : fip-stm32mp257f-ev1-ca35tdcid-ostl-optee-emmc.bin
10:00:43 : Size : 2.65 MB
10:00:43 : Partition ID : 0x03
10:00:43 : Download in Progress:
10:00:48 : aborting on going operation...
10:00:48 : Operation canceled
10:00:48 : Error: failed to download Segment[0]
10:00:48 : Error: failed to download the File
10:00:48 : Error: Download partition 0x03 failed
10:00:48 : Error: TSV flashing service failed
10:00:48 : Disconnected from device.

 

I have tried running the download for significantly longer (Current attempt has been 45 minutes) and it never seems to leave this loop. Any help would be greatly appreciated. 

This topic has been closed for replies.
CarsonBest answer
Associate III
September 18, 2024

Hi Oliver, 

 

I figured out that most of my problems stemmed from using ST link to supply power instead of the Jack. When I changed that the problems seemed to go away. Also switching to a linux machine helped. Thanks!

 

Carson

2 replies

Olivier GALLIEN
ST Technical Moderator
August 14, 2024

Hi @Carson ,

Can you please provide information about when and from who you get the board + share the reference you can find on the board and the SoC please. 

I assume you are using latest ecosystem V5.1 right ? 

Getting trace from UART during flashing operation can help to progress in analysis

Thanks 

OIivier 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
CarsonAuthorBest answer
Associate III
September 18, 2024

Hi Oliver, 

 

I figured out that most of my problems stemmed from using ST link to supply power instead of the Jack. When I changed that the problems seemed to go away. Also switching to a linux machine helped. Thanks!

 

Carson