Skip to main content
Visitor
Oct 5, 2026 8:05 AM UTC
Question

OpenSTLinux BSP security maintenance: CVE tracking, backports and Linux 6.1 support

Hello,

We are assessing security maintenance for an STM32MP1 product using linux-stm32mp. Could ST clarify the following?

  1. Is the maintenance policy in the 2021 "FAQ: Updating OpenSTLinux" (https://community.st.com/stm32-mpus-61/faq-updating-openstlinux-19) still current? How are security fixes delivered after a release: through component branches, tagged minor releases, or another mechanism? Has ST published updated guidance in preparation for the EU Cyber Resilience Act?

  2. Does ST assess kernel.org CNA CVEs against its vX.Y-stm32mp branches? Are per-CVE affected/fixed decisions published anywhere, such as a vulnerability list, VEX document, or CVE_STATUS entries in meta-st-stm32mp?

  3. For security vulnerabilities in ST-specific kernel changes that have not been upstreamed, what is the CVE assignment and advisory process? Where are fixes announced?

  4. The FAQ describes 1.5 years of feature development, 2.5 years of corrections, and a possible additional year of vulnerability-related releases. Which BSP components does this cover, including Linux and U-Boot? Is there a published lifecycle table showing support phases and end dates for each OpenSTLinux release?

  5. Is the v6.1-stm32mp branch still maintained? Are security updates planned beyond r2.1 (Linux 6.1.82), and should users expect selected backports or updates to newer upstream 6.1.y baselines?

Thank you.

1 reply

Kevin HUBER
ST Employee
Oct 28, 2026 3:41 PM UTC

Hello ​@um-itx ,

Did you see this page on the wiki ?
https://wiki.st.com/stm32mpu/wiki/Deep_dive_on_EU_CRA_for_STM32_MPU

BR,
Kevin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.