Skip to main content
darla14
Associate III
May 30, 2022
Solved

Not able to configure DMA1/2 with the USART2 in CM4 mode

Hello,

I am trying to associate the DMA1 in M4 context with USART2 but whenever I click "add" on the right pane, I see no USART2 on that, on the contrary, I see UART4 it on DMA2 as shown below. If I try to put DMA2 in M4 context, UART4 now appears in DMA1 and I cannot Assign both of them to M4

 

0693W00000NqqWAQAZ.png 

 

No uart/usart when i click add , please see below image :

0693W00000NqqXDQAZ.png 

 

0693W00000NqqXNQAZ.png 

My aim is to associate the USART2 with the DMA1 if it is possible. Please guide.

Regards,

D

 

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
May 30, 2022

Hi @darla14​ ,

first, I encourage you to stick with our default usage of DMA1 to A7NS and DMA2 to M4

Did you assign the USART2 to M4 runtime context ?

0693W00000NqrpNQAR.pngOn my side, seems to work as expected.

0693W00000NqrpIQAR.pngRegards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

2 replies

PatrickF
PatrickFBest answer
ST Employee
May 30, 2022

Hi @darla14​ ,

first, I encourage you to stick with our default usage of DMA1 to A7NS and DMA2 to M4

Did you assign the USART2 to M4 runtime context ?

0693W00000NqrpNQAR.pngOn my side, seems to work as expected.

0693W00000NqrpIQAR.pngRegards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
darla14
darla14Author
Associate III
May 30, 2022

@PatrickF​  Thanks , assigning USART2 to M4 and then assigning DMA2 can see USART2 in that.

Thanks a lot !

br,

D