Skip to main content
BSunw.1
Associate III
February 5, 2021
Question

New M4 project in cubeide has build button grayed out while running distribution package on STM32MP157c-DK2?

I am running the st-example-image-qt distribution package and am trying to use the M4 processor to feed sensor data to my UI. I can import the OpenAMP_TTY_echo example into stm32cubeide and debug it with my board fine. But now I am trying to make my own project since the OpenAMP example does not have a .ioc configuration file and I would like to set up some timer interrupts and things. Looking in the OpenAMP example, the timer HAL files are not even in there.

So I created a new project and selected the STM32MP157c-DK2. It loaded a .ioc configuration file but the project will not build. I don't think there is a build file but I thought that was generated automatically? I can add a debug configuration but there is no .elf to link to.

What would be the easiest way to move forward?

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
February 8, 2021

Hi @BSunw.1​ ,

Do you well select and have focus on the _CM4 sub-project when you attempt to build ?

Else could you please share a screen shot of your CubeIDE "Project Explorer" when hammer button is grayed ?

Thx

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
BSunw.1
BSunw.1Author
Associate III
March 1, 2021

Hi @Community member​ ,

Yeah I have tried it with the main.c file opened and various directories selected but can't seem to get the build button to be clickable.

0693W000007Zi4ZQAS.png