Skip to main content
Sxx
Associate
August 27, 2025
Question

Linker file example for STM32MP135 bare metal project based on Keil RTX v5.6.0

Hello everyone.

I'm developing a bare metal project on STM32mp135F-DK using Keil RTX5 operating system.

Actually I'm using the default "stm32mp13xx_a7_ddr.ld" finded in SDK, but in it no RTX related section are indicated.

 

I'm working with:

STM32CubeIDE

Version: 1.19.0

Build: 25607_20250703_0907 (UTC)

 

Can anyone help me with an example of loader file to use?

How indicate the 8 byte aligned section necessary to RTX for stack and heap threads?

It's necessary particular settings for MMU and CACHE?

 

Thanks in advance.

 

 

This topic has been closed for replies.