Skip to main content
Associate
January 6, 2024
Solved

Issues installing developer package

Hi,

I've been following along with the "Getting started" on the wiki, but I cannot set up the developer package for my STM32MP157x-DK2. Downloading the file and trying to extract the archives, I get the following:

```

adriaan@ZOBLZO21X5GY3:~$ cd STM32MPU_workspace/tmp/
adriaan@ZOBLZO21X5GY3:~/STM32MPU_workspace/tmp$ ll
total 667536
drwxr-xr-x 2 adriaan adriaan 4096 Jan 6 16:49 ./
drwxr-xr-x 4 adriaan adriaan 4096 Jan 5 16:23 ../
-rw-r--r-- 1 adriaan adriaan 262113357 Jan 6 16:45 en.SDK-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz
-rw-r--r-- 1 adriaan adriaan 50 Jan 6 16:45 en.SDK-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz:Zone.Identifier
-rw-r--r-- 1 adriaan adriaan 421422061 Jan 6 16:46 en.flash-stm32mp1-openstlinux-6-1-yocto-mickledore-mp1-v23-06-21.tar.gz
-rw-r--r-- 1 adriaan adriaan 50 Jan 6 16:46 en.flash-stm32mp1-openstlinux-6-1-yocto-mickledore-mp1-v23-06-21.tar.gz:Zone.Identifier
adriaan@ZOBLZO21X5GY3:~/STM32MPU_workspace/tmp$ tar xvf en.SDK-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz
stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/
stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/sdk/
stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.host.manifest
stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21-license_content.html
stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.license
stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.sh

gzip: stdin: unexpected end of file
tar: Unexpected EOF in archive
tar: Unexpected EOF in archive
tar: Error is not recoverable: exiting now

```

I've tried multiple versions of the release.

I am working on WSL2 (Ubuntu 20.04), Windows 11.

I've also tried to use VMWare, but the result is the same...

 

Please assist.

This topic has been closed for replies.
Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
ST Technical Moderator
January 8, 2024

@adriaan-mernok ,
I asked some of my colleagues to do the same test, but nobody fall on this error, I am really sorry that we cannot give many help as I have no idea of what can happen on your side. Is it possible that you work on an industrial Internet network that can block downloading above a maximum size ?

Please when you download your tarball, check the size with the following command :

 PC $> ls -la

Output : 
-rw-r--r-- 1 <...> <...> -ps 817627492 Jan  8 13:21 en.SDK-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

6 replies

Erwan SZYMANSKI
ST Technical Moderator
January 8, 2024

Hello @adriaan-mernok ,
I am sorry to hear it but we tested it this morning on different PCs on our side after seeing your message, but we could not have reproduced your issue. Maybe it can be caused by your own PC configuration ?

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
January 8, 2024

Hi @Erwan SZYMANSKI, thanks for the reply.

 

I've also downloaded it with a different browser (initially Brave, now Edge).

Copied the file via SSH to a different device (RPI CM4 running headless Raspbian), but the issue persists.

Downloaded the file here:
STM32MP1Dev - STM32MP1 OpenSTLinux Developer Package - STMicroelectronics

Yocto_SDKx86

 

I am stumped as to what could be causing this.

Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
ST Technical Moderator
January 8, 2024

@adriaan-mernok ,
I asked some of my colleagues to do the same test, but nobody fall on this error, I am really sorry that we cannot give many help as I have no idea of what can happen on your side. Is it possible that you work on an industrial Internet network that can block downloading above a maximum size ?

Please when you download your tarball, check the size with the following command :

 PC $> ls -la

Output : 
-rw-r--r-- 1 <...> <...> -ps 817627492 Jan  8 13:21 en.SDK-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.